IMX8QM MCLKOUT0 Frequency Modify

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX8QM MCLKOUT0 Frequency Modify

1,727件の閲覧回数
smarter
Contributor II

Hi,

        Our designed board use cs4345 ,some features like wm8524,use IMX8QM_AUD_MCLKOUT0 as mclk input . driver is like wm8524 too. mclk frequency is 128800, is not 2457600,how can i change this issue.

ラベル(1)
0 件の賞賛
返信
1 返信

1,657件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi bin

general approach can be check dts file for "IMX8QM_AUD_MCLKO" and clock driver

fsl-imx8qm-mek.dtsi\freescale\dts\boot\arm64\arch - linux-imx - i.MX Linux kernel 

clk-imx8qm.c\imx\clk\drivers - linux-imx - i.MX Linux kernel 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信