IMX8QM MCLKOUT0 Frequency Modify

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8QM MCLKOUT0 Frequency Modify

1,710 Views
smarter
Contributor II

Hi,

        Our designed board use cs4345 ,some features like wm8524,use IMX8QM_AUD_MCLKOUT0 as mclk input . driver is like wm8524 too. mclk frequency is 128800, is not 2457600,how can i change this issue.

0 Kudos
Reply
1 Reply

1,640 Views
igorpadykov
NXP Employee
NXP Employee

Hi bin

general approach can be check dts file for "IMX8QM_AUD_MCLKO" and clock driver

fsl-imx8qm-mek.dtsi\freescale\dts\boot\arm64\arch - linux-imx - i.MX Linux kernel 

clk-imx8qm.c\imx\clk\drivers - linux-imx - i.MX Linux kernel 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply