IMX8MQ Android 9.0.2 screen turned to 180, the video playback did not turn to 180.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX8MQ Android 9.0.2 screen turned to 180, the video playback did not turn to 180.

2,633件の閲覧回数
Tico
Contributor II

IMX8MQ  Android 9.0.1 and  9.0.2 screen turned to 180,

the video playback did not turn to 180.

Use this command:
"settings put system user_rotation 2"

Can someone help improve this problem?

p3.jpg

p2.jpg

0 件の賞賛
返信
3 返答(返信)

2,389件の閲覧回数
owen_wen
Contributor III

Hi Tico,

I got the same problem, did you find the solution or work around now?

0 件の賞賛
返信

2,406件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Hello

To rotation the screen, you can add followed two lines in init.rc, both video and GUI are rotated.

 

  setprop persist.demo.rotationlock true
  setprop persist.demo.remoterotation portrait 

 
Hope this information could help you.
Best regards,
Diego.
0 件の賞賛
返信

2,406件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Hello,

This is a known issue. Let me report this internally to see if already exist a solution for this problem.

Best regards,

Diego.

0 件の賞賛
返信