IMX8MP build error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX8MP build error

3,797 次查看
yenchou
Contributor III

Hi ALL,

version : imx-android-11.0.0_2.0.0

platform : IMX8MP

I followed the "android-11.0.0_2.0.0 — 22 April 2021  User's Guide" to build image, but the log show a error.

ERROR: fopen imx-android-11.0.0_2.0.0/android_build/vendor/nxp-opensource/arm-trusted-firmware/build/imx8mp/release: No such file or directory

ld.lld: error: cannot open @sound/soc/codecs/snd-soc-bt-sco.o.in: No such file or directory

ld.lld: error: cannot open @drivers/clk/imx/mxc-clk.o.in: No such file or directory

ld.lld: error: cannot open @drivers/clk/imx/mxc-clk.o.in: No such file or directory

Please tell me  how to solve the problem ?

 

Thank you.

Best Wishes

 

0 项奖励
回复
8 回复数

3,784 次查看
jimmychan
NXP TechSupport
NXP TechSupport

Have you run this command : source ~/imx-android-11.0.0_2.0.0/imx_android_setup.sh

0 项奖励
回复

3,782 次查看
yenchou
Contributor III

Yes, I have run the command.

When I try to change the git tag "android-11.0.0_2.0.0" to "android-11.0.0_1.2.0", the error don't occur.

Could I use the git tag "android-11.0.0_1.2.0" to build the android-11.0.0_2.0.0 image?

0 项奖励
回复

3,767 次查看
jimmychan
NXP TechSupport
NXP TechSupport

It is better to download the source package for Android 11.0.0_1.2.0. This version is for i.MX8MP.

https://www.nxp.com/design/software/embedded-software/i-mx-software/android-os-for-i-mx-applications...

 

 

0 项奖励
回复

3,763 次查看
yenchou
Contributor III

Hi  Jimmychan,

Because  the  android-11.0.0_2.0.0 release note say upgraded the kernel from v5.4.47 to v5.10.9, I would like to use the new Linux kernel version.

Could other methods to debug the issue?

 

 

0 项奖励
回复

3,726 次查看
jimmychan
NXP TechSupport
NXP TechSupport

I tried to build the android-11.0.0_2.0.0. I don't have any error.

Please try to clean up your host and then build it again.

0 项奖励
回复

3,717 次查看
yenchou
Contributor III

I tried to build the android-11.0.0_1.2.1 and don't have any error.

But the android-11.0.0_2.0.0 remains to build error.

What package does NXP recommend version on i.mx8mp ?

0 项奖励
回复

3,702 次查看
jimmychan
NXP TechSupport
NXP TechSupport

It is up to customer which version they want to use. Maybe you try to upgrade the version of the compiler on your host.  

0 项奖励
回复

3,691 次查看
yenchou
Contributor III

I used the gcc-arm-10.2-2020.11-x86_64-aarch64-none-linux-gnu compiler to build  imx-android-11.0.0_2.0.0, but it build error again.

I try to lunch  evk_8mm-userdebug and it get the same error.

Below is my step:

$ mkdir ~/bin
$ curl https://storage.googleapis.com/git-repo-downloads/repo > ~/bin/repo
$ chmod a+x ~/bin/repo
$ export PATH=${PATH}:~/bin
$ source imx-android-11.0.0_2.0.0/imx_android_setup.sh
$ export MY_ANDROID=`pwd`
$export AARCH64_GCC_CROSS_COMPILE=/opt/gcc-arm-10.2-2020.11-x86_64-aarch64-none-linux-gnu//bin/aarch64-linux-gnu-
$ cd ${MY_ANDROID}
$ source build/envsetup.sh
$ lunch evk_8mp-userdebug
$ ./imx-make.sh -j4 2>&1 | tee build-log.txt

Below is the error log:

make[1]: Leaving directory `/home/user/imx8mp-android-11.0.0_2.0.0/android_build/vendor/nxp-opensource/arm-trusted-firmware'
Makefile:1276: warning: overriding commands for target `/home/user/imx8mp-android-11.0.0_2.0.0/android_build/vendor/nxp-opensource/arm-trusted-firmware/build/imx8mm/release'
Makefile:525: warning: ignoring old commands for target `/home/user/imx8mp-android-11.0.0_2.0.0/android_build/vendor/nxp-opensource/arm-trusted-firmware/build/imx8mm/release'
ERROR: fopen /home/user/imx8mp-android-11.0.0_2.0.0/android_build/vendor/nxp-opensource/arm-trusted-firmware/build/imx8mm/release: No such file or directory
make[1]: *** [/home/user/imx8mp-android-11.0.0_2.0.0/android_build/vendor/nxp-opensource/arm-trusted-firmware/build/imx8mm/release] Error 1
make: *** [/home/user/imx8mp-android-11.0.0_2.0.0/android_build/out/target/product/evk_8mm/u-boot.imx] Error 1

 I build the imx-android-11.0.0_1.2.1, but it dose not have any error.

So I think that it is not  the compiler version problem.

Could other method solve the problem ?

0 项奖励
回复