IMX8MP build error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8MP build error

4,162 Views
yenchou
Contributor III

Hi ALL,

version : imx-android-11.0.0_2.0.0

platform : IMX8MP

I followed the "android-11.0.0_2.0.0 — 22 April 2021  User's Guide" to build image, but the log show a error.

ERROR: fopen imx-android-11.0.0_2.0.0/android_build/vendor/nxp-opensource/arm-trusted-firmware/build/imx8mp/release: No such file or directory

ld.lld: error: cannot open @sound/soc/codecs/snd-soc-bt-sco.o.in: No such file or directory

ld.lld: error: cannot open @drivers/clk/imx/mxc-clk.o.in: No such file or directory

ld.lld: error: cannot open @drivers/clk/imx/mxc-clk.o.in: No such file or directory

Please tell me  how to solve the problem ?

 

Thank you.

Best Wishes

 

0 Kudos
Reply
8 Replies

4,149 Views
jimmychan
NXP TechSupport
NXP TechSupport

Have you run this command : source ~/imx-android-11.0.0_2.0.0/imx_android_setup.sh

0 Kudos
Reply

4,147 Views
yenchou
Contributor III

Yes, I have run the command.

When I try to change the git tag "android-11.0.0_2.0.0" to "android-11.0.0_1.2.0", the error don't occur.

Could I use the git tag "android-11.0.0_1.2.0" to build the android-11.0.0_2.0.0 image?

0 Kudos
Reply

4,132 Views
jimmychan
NXP TechSupport
NXP TechSupport

It is better to download the source package for Android 11.0.0_1.2.0. This version is for i.MX8MP.

https://www.nxp.com/design/software/embedded-software/i-mx-software/android-os-for-i-mx-applications...

 

 

0 Kudos
Reply

4,128 Views
yenchou
Contributor III

Hi  Jimmychan,

Because  the  android-11.0.0_2.0.0 release note say upgraded the kernel from v5.4.47 to v5.10.9, I would like to use the new Linux kernel version.

Could other methods to debug the issue?

 

 

0 Kudos
Reply

4,091 Views
jimmychan
NXP TechSupport
NXP TechSupport

I tried to build the android-11.0.0_2.0.0. I don't have any error.

Please try to clean up your host and then build it again.

0 Kudos
Reply

4,082 Views
yenchou
Contributor III

I tried to build the android-11.0.0_1.2.1 and don't have any error.

But the android-11.0.0_2.0.0 remains to build error.

What package does NXP recommend version on i.mx8mp ?

0 Kudos
Reply

4,067 Views
jimmychan
NXP TechSupport
NXP TechSupport

It is up to customer which version they want to use. Maybe you try to upgrade the version of the compiler on your host.  

0 Kudos
Reply

4,056 Views
yenchou
Contributor III

I used the gcc-arm-10.2-2020.11-x86_64-aarch64-none-linux-gnu compiler to build  imx-android-11.0.0_2.0.0, but it build error again.

I try to lunch  evk_8mm-userdebug and it get the same error.

Below is my step:

$ mkdir ~/bin
$ curl https://storage.googleapis.com/git-repo-downloads/repo > ~/bin/repo
$ chmod a+x ~/bin/repo
$ export PATH=${PATH}:~/bin
$ source imx-android-11.0.0_2.0.0/imx_android_setup.sh
$ export MY_ANDROID=`pwd`
$export AARCH64_GCC_CROSS_COMPILE=/opt/gcc-arm-10.2-2020.11-x86_64-aarch64-none-linux-gnu//bin/aarch64-linux-gnu-
$ cd ${MY_ANDROID}
$ source build/envsetup.sh
$ lunch evk_8mp-userdebug
$ ./imx-make.sh -j4 2>&1 | tee build-log.txt

Below is the error log:

make[1]: Leaving directory `/home/user/imx8mp-android-11.0.0_2.0.0/android_build/vendor/nxp-opensource/arm-trusted-firmware'
Makefile:1276: warning: overriding commands for target `/home/user/imx8mp-android-11.0.0_2.0.0/android_build/vendor/nxp-opensource/arm-trusted-firmware/build/imx8mm/release'
Makefile:525: warning: ignoring old commands for target `/home/user/imx8mp-android-11.0.0_2.0.0/android_build/vendor/nxp-opensource/arm-trusted-firmware/build/imx8mm/release'
ERROR: fopen /home/user/imx8mp-android-11.0.0_2.0.0/android_build/vendor/nxp-opensource/arm-trusted-firmware/build/imx8mm/release: No such file or directory
make[1]: *** [/home/user/imx8mp-android-11.0.0_2.0.0/android_build/vendor/nxp-opensource/arm-trusted-firmware/build/imx8mm/release] Error 1
make: *** [/home/user/imx8mp-android-11.0.0_2.0.0/android_build/out/target/product/evk_8mm/u-boot.imx] Error 1

 I build the imx-android-11.0.0_1.2.1, but it dose not have any error.

So I think that it is not  the compiler version problem.

Could other method solve the problem ?

0 Kudos
Reply