IMX8MP Uboot

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
5,805件の閲覧回数
AsadNawaZ_93
Contributor II

My bootloader stucks here.

U-Boot SPL 2022.04-lf_v2022.04+g16e8414193 (Oct 08 2022 - 13:33:43 +0000)
No pca9450@25
DDRINFO: start DRAM init
DDRINFO: DRAM rate 3000MTS
DDRINFO:ddrphy calibration done
DDRINFO: ddrmix config done
Normal Boot
Trying to boot from BOOTROM
Boot Stage: Primary boot
image offset 0x8000, pagesize 0x200, ivt offset 0x0
Can't support legacy image
SPL: failed to boot from all boot devices

ERROR ### Please RESET the board

###############################################

タグ(1)
0 件の賞賛
返信
1 解決策
5,729件の閲覧回数
AsadNawaZ_93
Contributor II

Thanks for your reply. I have found the solution already. It was an issue of wrong UART address for ATF "ATF_BOOT_UART_BASE". After setting it correctly as per the UART address on carrier board (Renasas SMARC), I got it working.

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
5,730件の閲覧回数
AsadNawaZ_93
Contributor II

Thanks for your reply. I have found the solution already. It was an issue of wrong UART address for ATF "ATF_BOOT_UART_BASE". After setting it correctly as per the UART address on carrier board (Renasas SMARC), I got it working.

0 件の賞賛
返信
5,784件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信
5,776件の閲覧回数
AsadNawaZ_93
Contributor II

Thanks for your reply. Please find the detailed explanation in one of my other ticket. 

https://community.nxp.com/t5/i-MX-Processors/U-boot-Bootloader-not-loading-for-ADLINK-LEC-IMX8MP/td-...

 

0 件の賞賛
返信
5,771件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

I've replied to you in that tread, what media do you use? SD card?

0 件の賞賛
返信