[IMX8MP] How to apply RT patches into NXP's yocto distribution?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[IMX8MP] How to apply RT patches into NXP's yocto distribution?

1,112 Views
Airbus_A320
Contributor II

Hi,

we are evaluating, for our project, if we need Linux fully preemptible to reduce the scheduling jitter.

We have developed a SoM based on the IMX8MP EVK, a carrier board with the peripherals we need, and developed a stub of our software system as a proof of concept.

The system is working as intended, but occasionally we have some glitches due to latency spikes, sometimes in the tens of milliseconds range. 

When we started the development the latest Yocto Project User's Guide revision was IMXLXYOCTOUG v.LF5.15.71_2.2.0, and we are still using the same package versions. (I'm afraid that we are late to start again with a new kernel and BSP revision)

I managed to merge the patches rt51 from (https://mirrors.edge.kernel.org/pub/linux/kernel/projects/rt/5.15/older/) but the build is failing on some driver code. Am I missing some patches from NXP meant to be added on top of the rt51 patch set?

How can I enable full RT capabilities?

Thanks in advance for the support.

Tags (1)
0 Kudos
Reply
2 Replies

1,083 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport
0 Kudos
Reply

1,033 Views
Airbus_A320
Contributor II
This is not that helpful. It's just the same question from a year ago still without an answer...