[IMX8MP] DemoExperience GUI doesn't works on Yocto 4.0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[IMX8MP] DemoExperience GUI doesn't works on Yocto 4.0

1,017件の閲覧回数
mayqueen
Contributor IV

OS: Yocto 4.0

Kernel: 5.15.71

 

As title, that strange when I compile image on my host side, boot up works but when I open NXP demo experience, it's emtpy... Even if I change to command line mode using 'demoexperience tui' commnad, also showing No demos. So I check something as following:

1. /home/root/.nxp-demo-experience/ is exist in my rootfs

2. Execute demo under /home/root/.nxp-demo-experience/ one by one, it works perfectly, for exmaple:

python3 /home/root/.nxp-demo-experience/scripts/machine_learning/MLDemoLauncher.py detect (works)

3. Use strace to check something wrong or not, but it seems no problem:

openat(AT_FDCWD, "/etc/ld.so.cache", O_RDONLY|O_CLOEXEC) = 3
openat(AT_FDCWD, "/lib/libncurses.so.5", O_RDONLY|O_CLOEXEC) = 3
openat(AT_FDCWD, "/lib/libtinfo.so.5", O_RDONLY|O_CLOEXEC) = 3
openat(AT_FDCWD, "/usr/lib/libpanel.so.5", O_RDONLY|O_CLOEXEC) = 3
openat(AT_FDCWD, "/usr/lib/libQt6Gui.so.6", O_RDONLY|O_CLOEXEC) = 3
openat(AT_FDCWD, "/usr/lib/libQt6Qml.so.6", O_RDONLY|O_CLOEXEC) = 3
openat(AT_FDCWD, "/usr/lib/libQt6Network.so.6", O_RDONLY|O_CLOEXEC) = 3
openat(AT_FDCWD, "/usr/lib/libQt6Core.so.6", O_RDONLY|O_CLOEXEC) = 3
openat(AT_FDCWD, "/usr/lib/libstdc++.so.6", O_RDONLY|O_CLOEXEC) = 3
openat(AT_FDCWD, "/lib/libgcc_s.so.1", O_RDONLY|O_CLOEXEC) = 3
openat(AT_FDCWD, "/lib/libc.so.6", O_RDONLY|O_CLOEXEC) = 3
openat(AT_FDCWD, "/usr/lib/libGLESv2.so.2", O_RDONLY|O_CLOEXEC) = 3
openat(AT_FDCWD, "/usr/lib/libEGL.so.1", O_RDONLY|O_CLOEXEC) = 3
openat(AT_FDCWD, "/usr/lib/libfontconfig.so.1", O_RDONLY|O_CLOEXEC) = 3
openat(AT_FDCWD, "/usr/lib/libglib-2.0.so.0", O_RDONLY|O_CLOEXEC) = 3
openat(AT_FDCWD, "/usr/lib/libQt6DBus.so.6", O_RDONLY|O_CLOEXEC) = 3
openat(AT_FDCWD, "/usr/lib/libxkbcommon.so.0", O_RDONLY|O_CLOEXEC) = 3
openat(AT_FDCWD, "/usr/lib/libpng16.so.16", O_RDONLY|O_CLOEXEC) = 3
openat(AT_FDCWD, "/usr/lib/libharfbuzz.so.0", O_RDONLY|O_CLOEXEC) = 3
openat(AT_FDCWD, "/usr/lib/libfreetype.so.6", O_RDONLY|O_CLOEXEC) = 3
openat(AT_FDCWD, "/lib/libz.so.1", O_RDONLY|O_CLOEXEC) = 3
openat(AT_FDCWD, "/lib/libm.so.6", O_RDONLY|O_CLOEXEC) = 3
openat(AT_FDCWD, "/usr/lib/libzstd.so.1", O_RDONLY|O_CLOEXEC) = 3
openat(AT_FDCWD, "/usr/lib/libicui18n.so.70", O_RDONLY|O_CLOEXEC) = 3
openat(AT_FDCWD, "/usr/lib/libicuuc.so.70", O_RDONLY|O_CLOEXEC) = 3
openat(AT_FDCWD, "/usr/lib/libpcre2-16.so.0", O_RDONLY|O_CLOEXEC) = 3
openat(AT_FDCWD, "/usr/lib/libGAL.so", O_RDONLY|O_CLOEXEC) = 3
openat(AT_FDCWD, "/usr/lib/libVSC.so", O_RDONLY|O_CLOEXEC) = 3
openat(AT_FDCWD, "/usr/lib/libwayland-server.so.0", O_RDONLY|O_CLOEXEC) = 3
openat(AT_FDCWD, "/usr/lib/libwayland-client.so.0", O_RDONLY|O_CLOEXEC) = 3
openat(AT_FDCWD, "/usr/lib/libdrm.so.2", O_RDONLY|O_CLOEXEC) = 3
openat(AT_FDCWD, "/usr/lib/libgbm.so.1", O_RDONLY|O_CLOEXEC) = 3
openat(AT_FDCWD, "/usr/lib/libgbm_viv.so", O_RDONLY|O_CLOEXEC) = 3
openat(AT_FDCWD, "/usr/lib/libexpat.so.1", O_RDONLY|O_CLOEXEC) = 3
openat(AT_FDCWD, "/usr/lib/libuuid.so.1", O_RDONLY|O_CLOEXEC) = 3
openat(AT_FDCWD, "/usr/lib/libpcre.so.1", O_RDONLY|O_CLOEXEC) = 3
openat(AT_FDCWD, "/usr/lib/libdbus-1.so.3", O_RDONLY|O_CLOEXEC) = 3
openat(AT_FDCWD, "/lib/libpthread.so.0", O_RDONLY|O_CLOEXEC) = 3
openat(AT_FDCWD, "/usr/lib/libicudata.so.70", O_RDONLY|O_CLOEXEC) = 3
openat(AT_FDCWD, "/usr/lib/libffi.so.8", O_RDONLY|O_CLOEXEC) = 3
openat(AT_FDCWD, "/lib/libsystemd.so.0", O_RDONLY|O_CLOEXEC) = 3
openat(AT_FDCWD, "/lib/libcap.so.2", O_RDONLY|O_CLOEXEC) = 3
openat(AT_FDCWD, "/etc/terminfo/l/linux", O_RDONLY) = 3
openat(AT_FDCWD, "/home/root/.nxp-demo-experience/demos.json", O_RDONLY|O_CLOEXEC) = 3

 

Any idea? I think just missing a bit stuff, need some directions, thanks!

ラベル(2)
0 件の賞賛
返信
1 返信

976件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Apparently is bad download of demoexperience since all this issue is due to your host, i suggest to erase everything and download and burn again to see what happen.

Regards

0 件の賞賛
返信