IMX8MN USB OTG not recognized (when doing ddr test)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

IMX8MN USB OTG not recognized (when doing ddr test)

跳至解决方案
2,109 次查看
AccuJie
Contributor III

Hi

We have three customized IMX8MN boards. Now, we are trying to do the ddr training & stress test.

However, two of our boards are not recognized by the PC at all. Another one just got a warning of USB device not recognized. We already changed the boot mode to serial download mode.

AccuJie_0-1637092330741.png

 

Of cause we got the error inside ddr training and stress test tools:

ERROR: Can't open USB device!!!
Please check if the correct target is selected and set to the serial download mode

 

We are using the PMIC of PCA9450 with a 2Gb DDR4. Here is the power rail supply from the pmic I measured(when in serial download mode before firmware download):

VSYS_5V5V
PCA9450B_BUCK1(VDD_SOC&VDD_DRAM)0.85V
PCA9450B_BUCK2(VDD_ARM)0.85V
PCA9450B_BUCK4(VDD_3V3/NVCC_3V3)3.3V
PCA9450B_BUCK5(VDD_1v8/NVCC_1V8)1.8V
PCA9450B_BUCK6(NVCC_DRAM)1.1V
PCA9450B_LDO1(NVCC_SNVS_1V8)1.78V
PCA9450B_LDO2(VDD_SNVS_0V8 )0.8V
PCA9450B_LDO3(1V8_VDDA)1.8V

Base on my understanding, the firmware download in ddr test tools(download into on-chip internal RAM) only needs the basic voltage(default config).

Where should I have a check in the next step?

Thanks.

0 项奖励
回复
1 解答
2,102 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Jie

 

for that issue one can check sect.Table 8. USB recommendations, clock stability

using sect.Table 10. Oscillator/Crystal recommendations     i.MX 8M Nano Hardware Developer’s Guide

 

Best regards
igor

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,103 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Jie

 

for that issue one can check sect.Table 8. USB recommendations, clock stability

using sect.Table 10. Oscillator/Crystal recommendations     i.MX 8M Nano Hardware Developer’s Guide

 

Best regards
igor

0 项奖励
回复
2,083 次查看
AccuJie
Contributor III

Thanks for your suggestion. We found out that the problem is from our oscillator. 

0 项奖励
回复