IMX8MN :- Disable automatic login application : hwrng

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8MN :- Disable automatic login application : hwrng

3,336 Views
milav_soni
Contributor III

Hello all,

I have build an image for imx8mnano based custom board.

I have use "imx-linux-zeus -m imx-5.4.70-2.3.2.xml" bsp to generate an image.

When I power up my board and login in to console, following log are arriving continuously.

root@imx8mnevk:~# [   42.723982] caam_jr 30901000.jr: 20000256: CCB: desc idx 2: RNG: Prediction resistance
[   42.731926] hwrng: no data available
[   52.963975] caam_jr 30901000.jr: 20000256: CCB: desc idx 2: RNG: Prediction resistance
[   52.971921] hwrng: no data available
[   63.203998] caam_jr 30901000.jr: 20000256: CCB: desc idx 2: RNG: Prediction resistance
[   63.211943] hwrng: no data available

I want to stop this application from kernel source.

can you please help me to find this content?

Thank You

Labels (1)
0 Kudos
Reply
4 Replies

2,684 Views
linderpi
Contributor II

I have the same problem on an i.MX 8M Mini after introducing OP-TEE. Have you guys found a solution in the meantime?

0 Kudos
Reply

3,314 Views
milav_soni
Contributor III

I have commented above kernel message in their respected files.

But I don't know how to disable the application.

Thank You

0 Kudos
Reply

3,330 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello milav,

Please check this link where auto login was disable:

https://community.nxp.com/t5/i-MX-Processors/Reg-Auto-Login-and-run-a-script-Automatically/m-p/28926...

 

Regards

 

0 Kudos
Reply

3,321 Views
trk_golf
Contributor I

Having same issue on imx8mm.

Not sure how auto-login solves the issue with the hardware random number generator.

@Bio_TICFSL, is there something more specific to help correct the root cause of these kernel messages?

0 Kudos
Reply