IMX 6 Solo Free run clock

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX 6 Solo Free run clock

356 Views
DK4509
Contributor II

Hi,

I am planning to provide on the CLK1_P/N pins a 133MHz clock of the IMX 6 solo processor.

Can I get a core clock frequency output, near to 1GHz if 133MHz is provided to CLK1_P/N signals?

If so, how will the calculation be determined on?

Thanks,

Dinesh

Screenshot 2023-01-20 155418.png

0 Kudos
Reply
1 Reply

303 Views
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hi @DK4509,

I hope you are doing well.

Please refer to the reference manual IMX6SDLRM section 18.5.1.3 PLL reference clock.
i.e For ARM PLL, the formula for PLL output frequency is
PLL output frequency = Fref * DIV_SEL/2


Here DIV_SEL is CCM_ANALOG_PLL_ARM[DIV_SELECT] bit.
and Fref is a reference clock.

Thanks & Regards,
Sanket Parekh

0 Kudos
Reply