IMX8MM USB Compliance

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX8MM USB Compliance

4,423 次查看
jonas_blick
Contributor I

Hi,

I seen serveral post on the tools/document needed for USB2.0 (HS eye) test for the IMX8Mini,

I also need this documents/files in order to do some compliance testing.

Thank you.

标签 (1)
0 项奖励
回复
6 回复数

3,767 次查看
hms1234
Contributor I

Hi

Can i get access to https://community.nxp.com/docs/DOC-329745 

/henrik

0 项奖励
回复

4,292 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Jonas

document was sent via mail.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

4,292 次查看
penny_lin
Contributor III

Hi igor:

  Could you share the document to me , I also need this documents/files in order to do some compliance testing.

Thank your help.

Penny Lin

0 项奖励
回复

4,292 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Penny 

suggest to create service request https://community.nxp.com/docs/DOC-329745 

Best regards
igor

0 项奖励
回复

4,133 次查看
christophapel
Contributor I

Hi Igor,

I would also need access to the necessary patches to run USB test mode.

access to https://community.nxp.com/docs/DOC-329745 is denied.

thanks and regards, Christoph

0 项奖励
回复

4,128 次查看
christophapel
Contributor I

to be precise, I have "I.MX6/7/8 series USB Certification Guide" available but cannot locate "How to do USB Compliance Test for 4.x kernel_v2.5" which is supposed to describe the necessary BSP patches.

0 项奖励
回复