IMX8MM: One SAI two i2S

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX8MM: One SAI two i2S

ソリューションへジャンプ
2,208件の閲覧回数
denyslytvynov
Contributor I

Hello,

In the user manual under paragraph 13.9.1.2 there is a block diagram (Figure 13-104) which shows TX and RX signals which can be used for i2S. My question is:

I am trying to connect two devices - a Microphone and a Speaker. Both are using i2S for communication although one as a transmitter and another as a receiver. Microphone, MPN SPH0645LM4H-B, has WS, BCLK, DOUT and Speaker has a DAC - TAS2505 which is driven with i2S - WS, BLCK,  DIN. Would it be possible to drive both if I connect them in the following manner:
Microphone: 
  • WS - SAI2_RXFS
  • BCLK - SAI2_RXC
  • DOUT - SAI2_RXDO
Speaker:
  • WS - SAI2_TXFS
  • BCLK - SAI2_TXC
  • DIN - SAI2_TXD0

pastedImage_1.png

Kind Regards,
Den

タグ(3)
0 件の賞賛
返信
1 解決策
2,139件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Den

>Would it be possible to drive both if I connect them in the following manner..

yes such connection is possible

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,140件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Den

>Would it be possible to drive both if I connect them in the following manner..

yes such connection is possible

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信