IMX8MM: One SAI two i2S

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

IMX8MM: One SAI two i2S

跳至解决方案
2,187 次查看
denyslytvynov
Contributor I

Hello,

In the user manual under paragraph 13.9.1.2 there is a block diagram (Figure 13-104) which shows TX and RX signals which can be used for i2S. My question is:

I am trying to connect two devices - a Microphone and a Speaker. Both are using i2S for communication although one as a transmitter and another as a receiver. Microphone, MPN SPH0645LM4H-B, has WSBCLKDOUT and Speaker has a DAC - TAS2505 which is driven with i2S WSBLCK,  DIN. Would it be possible to drive both if I connect them in the following manner:
Microphone: 
  • WS - SAI2_RXFS
  • BCLK - SAI2_RXC
  • DOUT - SAI2_RXDO
Speaker:
  • WS - SAI2_TXFS
  • BCLK - SAI2_TXC
  • DIN - SAI2_TXD0

pastedImage_1.png

Kind Regards,
Den

标记 (3)
0 项奖励
回复
1 解答
2,118 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Den

>Would it be possible to drive both if I connect them in the following manner..

yes such connection is possible

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,119 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Den

>Would it be possible to drive both if I connect them in the following manner..

yes such connection is possible

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复