IMX8M booting options

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8M booting options

Jump to solution
1,823 Views
Luishernandez1
Contributor II

Hi everyone,

 

Want to confirm that the IMX8M Nano supports booting off the below linked NAND through the GPMI interface.

https://4donline.ihs.com/images/VipMasterIC/IC/FASL/FASLS03878/FASLS03878-1.pdf?hkey=52A5661711E4025...

 

Regards,

Israel H.

Labels (1)
0 Kudos
Reply
1 Solution
1,816 Views
nxf63675
NXP TechSupport
NXP TechSupport

Hi Luishernandez1,

 

Reviewing the datasheet from the NAND and the iIMX8M nano it should be compatible with no further problems, also one can check the reference manual on the chapter 6.1.5 Boot devices (internal boot), please take a look on the fragment from the manual:

- Raw NAND (MLC and SLC), and Toggle-mode NAND flash through GPMI-2
interface, located at CS0. Page sizes of 2 KB, 4 KB, and 8 KB. The bus widths of 8-
bit with 2 through 62-bit BCH hardware ECC (Error Correction) are supported.

 

Regards,

Israel H.

View solution in original post

0 Kudos
Reply
1 Reply
1,817 Views
nxf63675
NXP TechSupport
NXP TechSupport

Hi Luishernandez1,

 

Reviewing the datasheet from the NAND and the iIMX8M nano it should be compatible with no further problems, also one can check the reference manual on the chapter 6.1.5 Boot devices (internal boot), please take a look on the fragment from the manual:

- Raw NAND (MLC and SLC), and Toggle-mode NAND flash through GPMI-2
interface, located at CS0. Page sizes of 2 KB, 4 KB, and 8 KB. The bus widths of 8-
bit with 2 through 62-bit BCH hardware ECC (Error Correction) are supported.

 

Regards,

Israel H.

0 Kudos
Reply