IMX8M Plus camera noise reduction

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX8M Plus camera noise reduction

ソリューションへジャンプ
4,259件の閲覧回数
A_Hiroki
Contributor I

Hi Community!

The i.MX8M Plus reference manual states that the camera's ISP has a filter function to reduce noise.

・Denoising pre-filter
・Filter (Noise reduction)
・Enhanced Chroma Noise Reduction (CNR)

I have a few questions.

Which register should I operate to turn on these filters?
What exactly are these filters? Are there any formulas for calculating the filters?

Thank you in advance for your help

Best Regards,
Hiroki

ラベル(1)
0 件の賞賛
返信
1 解決策
4,231件の閲覧回数
khang_letruong
Senior Contributor III

Hi @A_Hiroki,

I am afraid that the algos relevant to the ISP on iMX8MP are not open to public.  You might need to ask the NXP FAE in your region.

Regards,
Khang

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
4,244件の閲覧回数
khang_letruong
Senior Contributor III

Hi @A_Hiroki,

You can try the VVEXT tool from the isp-imx framework (found in /opt/imx8-isp/bin/ on a running board) and investigate the source code of relevant elements in the pipelines (sensor, isp, dwe, ...) here : https://github.com/nxp-imx/isp-vvcam

Regards,
Khang

 

0 件の賞賛
返信
4,238件の閲覧回数
A_Hiroki
Contributor I

Hi, @khang_letruong 

Thanks.
On the other hand, is it possible to know somewhere what the noise reduction algorithm is?
I would like to use it to analyze images.

Regards,
Hiroki

 

 

0 件の賞賛
返信
4,232件の閲覧回数
khang_letruong
Senior Contributor III

Hi @A_Hiroki,

I am afraid that the algos relevant to the ISP on iMX8MP are not open to public.  You might need to ask the NXP FAE in your region.

Regards,
Khang

0 件の賞賛
返信