IMX8M Plus camera noise reduction

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8M Plus camera noise reduction

Jump to solution
1,062 Views
A_Hiroki
Contributor I

Hi Community!

The i.MX8M Plus reference manual states that the camera's ISP has a filter function to reduce noise.

・Denoising pre-filter
・Filter (Noise reduction)
・Enhanced Chroma Noise Reduction (CNR)

I have a few questions.

Which register should I operate to turn on these filters?
What exactly are these filters? Are there any formulas for calculating the filters?

Thank you in advance for your help

Best Regards,
Hiroki

0 Kudos
Reply
1 Solution
1,034 Views
khang_letruong
Senior Contributor III

Hi @A_Hiroki,

I am afraid that the algos relevant to the ISP on iMX8MP are not open to public.  You might need to ask the NXP FAE in your region.

Regards,
Khang

View solution in original post

0 Kudos
Reply
3 Replies
1,047 Views
khang_letruong
Senior Contributor III

Hi @A_Hiroki,

You can try the VVEXT tool from the isp-imx framework (found in /opt/imx8-isp/bin/ on a running board) and investigate the source code of relevant elements in the pipelines (sensor, isp, dwe, ...) here : https://github.com/nxp-imx/isp-vvcam

Regards,
Khang

 

0 Kudos
Reply
1,041 Views
A_Hiroki
Contributor I

Hi, @khang_letruong 

Thanks.
On the other hand, is it possible to know somewhere what the noise reduction algorithm is?
I would like to use it to analyze images.

Regards,
Hiroki

 

 

0 Kudos
Reply
1,035 Views
khang_letruong
Senior Contributor III

Hi @A_Hiroki,

I am afraid that the algos relevant to the ISP on iMX8MP are not open to public.  You might need to ask the NXP FAE in your region.

Regards,
Khang

0 Kudos
Reply