IMX8M Plus LPDDR4

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,938件の閲覧回数
Anderswikstrom
Contributor I

Hi,

Is it possible to only connect one channel (A or B) for IMX8M Plus, to interface a 16-bit LPDDR4 memory?

Br

Anders

0 件の賞賛
返信
1 解決策
1,930件の閲覧回数
Yuri
NXP Employee
NXP Employee

@Anderswikstrom 
Hello,

   generally, since LPDDR4 device consists of two identical channels operating independently, it is possible to configure single channel x16 mode.

   Below are discussions regarding the issue.

https://community.nxp.com/t5/i-MX-Processors/Single-channel-LPDDR4/m-p/818564

https://community.nxp.com/t5/i-MX-Processors/Supporting-single-channel-LPDDR4-on-iMX8MP/m-p/1387065

 

 

Regards,
Yuri.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,931件の閲覧回数
Yuri
NXP Employee
NXP Employee

@Anderswikstrom 
Hello,

   generally, since LPDDR4 device consists of two identical channels operating independently, it is possible to configure single channel x16 mode.

   Below are discussions regarding the issue.

https://community.nxp.com/t5/i-MX-Processors/Single-channel-LPDDR4/m-p/818564

https://community.nxp.com/t5/i-MX-Processors/Supporting-single-channel-LPDDR4-on-iMX8MP/m-p/1387065

 

 

Regards,
Yuri.

0 件の賞賛
返信