IMX8M-Mini CSI Interface max transfer rate

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX8M-Mini CSI Interface max transfer rate

ソリューションへジャンプ
2,666件の閲覧回数
quentin_rasmont
Contributor I

Hi all,

from the applications processor reference manual regarding the CSI interface, I read that :

- in MIPI CSI the support for video capture goes up to 1080p@60fps

- in a 4-lane MIPI CSI2 the support goes up to 5Mpixel@15fps

Could you confirm that therefore a 4K@30fps transfer rate in not possible ?

ラベル(1)
1 解決策
2,459件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Hello,

Technically, the 4K@30fps is supported, but just by the MIPI-CSI PHY. The i.MX8MM does not have the capability to support 4K resolution. 

Best regards,

Diego. 

元の投稿で解決策を見る

2 返答(返信)
2,460件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Hello,

Technically, the 4K@30fps is supported, but just by the MIPI-CSI PHY. The i.MX8MM does not have the capability to support 4K resolution. 

Best regards,

Diego. 

2,459件の閲覧回数
quentin_rasmont
Contributor I

Thanks!

0 件の賞賛
返信