IMX8M-Mini CSI Interface max transfer rate

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8M-Mini CSI Interface max transfer rate

Jump to solution
2,665 Views
quentin_rasmont
Contributor I

Hi all,

from the applications processor reference manual regarding the CSI interface, I read that :

- in MIPI CSI the support for video capture goes up to 1080p@60fps

- in a 4-lane MIPI CSI2 the support goes up to 5Mpixel@15fps

Could you confirm that therefore a 4K@30fps transfer rate in not possible ?

Labels (1)
1 Solution
2,458 Views
diegoadrian
NXP Employee
NXP Employee

Hello,

Technically, the 4K@30fps is supported, but just by the MIPI-CSI PHY. The i.MX8MM does not have the capability to support 4K resolution. 

Best regards,

Diego. 

View solution in original post

2 Replies
2,459 Views
diegoadrian
NXP Employee
NXP Employee

Hello,

Technically, the 4K@30fps is supported, but just by the MIPI-CSI PHY. The i.MX8MM does not have the capability to support 4K resolution. 

Best regards,

Diego. 

2,458 Views
quentin_rasmont
Contributor I

Thanks!

0 Kudos
Reply