IMX8M-MINI internal RTC implementation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX8M-MINI internal RTC implementation

2,303件の閲覧回数
AMBh
Contributor I

Hi team,

I do have an application where I want to use internal RTC of IMX8M-mini controller. I have used Yocto setup for the same.

Can you support how I can use internal RTC in my application

 

Thanks,

Madhuri

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,280件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

The MX8M Mini does not have an internal 32k ring oscillator, and does not support the use of a crystal. 

 

Please see the datasheet, Section 3.1.4:

The RTC_XTALI is used for low-frequency functions. It supplies the clock for wake-up circuit, power-down real time clock operation, and slow system and watch-dog counters. The clock input can only be connected to an external oscillator. RTC_XTALO should be directly connected to VDD_SNVS_0P8.

and Section 3.4.2:

An external 32.768 kHz oscillator is necessary.  

 

Regards

0 件の賞賛
返信

2,266件の閲覧回数
AMBh
Contributor I

Hi,

Thanks for the reply

Okay I got your point. I also used BD71847AMWV power management IC which has internal RTC. How to use it ? 

0 件の賞賛
返信