IMX8M-MINI internal RTC implementation

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX8M-MINI internal RTC implementation

2,196 次查看
AMBh
Contributor I

Hi team,

I do have an application where I want to use internal RTC of IMX8M-mini controller. I have used Yocto setup for the same.

Can you support how I can use internal RTC in my application

 

Thanks,

Madhuri

标签 (1)
0 项奖励
回复
2 回复数

2,173 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

The MX8M Mini does not have an internal 32k ring oscillator, and does not support the use of a crystal. 

 

Please see the datasheet, Section 3.1.4:

The RTC_XTALI is used for low-frequency functions. It supplies the clock for wake-up circuit, power-down real time clock operation, and slow system and watch-dog counters. The clock input can only be connected to an external oscillator. RTC_XTALO should be directly connected to VDD_SNVS_0P8.

and Section 3.4.2:

An external 32.768 kHz oscillator is necessary.  

 

Regards

0 项奖励
回复

2,159 次查看
AMBh
Contributor I

Hi,

Thanks for the reply

Okay I got your point. I also used BD71847AMWV power management IC which has internal RTC. How to use it ? 

0 项奖励
回复