IMX8 audio tunning tool source code support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8 audio tunning tool source code support

3,885 Views
dongyang12
Contributor I

Hi,

I plan to development the voice algorithm in the IMX8MM. the algorithm is like your Conversa Voice. I also need development the tuning tool for the algorithm. And I find that conversa have tunning tool. And I need the demo code that the Windows PC application how to  interaction with the Conversa software running on the processor. Could you provide the tuning tool source code and the code about windows PC how to communite with the software running in the IMX8.

0 Kudos
Reply
8 Replies

3,875 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Which version BSP are you using? For the i.MX8MM board are you using the NXP reference board or the board you designed yourself?

0 Kudos
Reply

3,862 Views
dongyang12
Contributor I

Hi,

"Real-time_Edge_v2.5_IMX8MM-LPDDR4-EVK.zip" this is the image what I used. And I  using the NXP reference board, the name is 8MMINI-BB.

0 Kudos
Reply

3,834 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

@dongyang12 I have confirmed with our expert team that

The conversa tuning tool cannot work with other voice solution. And we have no source code for sharing.

Customer may use different ways for the connection of tuning tool with EVK, some voice solution may use TCP/IP network. Or the host PC can run both voice-call client and the tuning Tool. Through a composite device, both applications share an USB connection for the audio streams and tuning communication.

Hope this can do help for you

Wish you have a nice day

0 Kudos
Reply

3,828 Views
dongyang12
Contributor I

Thanks your feedback.

1, And I want to know conversa tuning tool using which way to communicate between Windows PC and host. 

2, My requestment is that Windows PC can communicate with host in real time. For example, Windows PC generates a file, which can then be sent to the host folder/tmp/file in real time. And windows PC can get the host data in real time.

About this, do you have any demo code to share us.

0 Kudos
Reply

3,820 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Sorry about that we have no source code for sharing.

Wish you have a nice day

0 Kudos
Reply

3,842 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

I will confirm it for you and then give you update.

0 Kudos
Reply

3,856 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

For the Core board is the 8MMINILPD4-CPU?

0 Kudos
Reply

3,843 Views
dongyang12
Contributor I

Yes.

0 Kudos
Reply