i.MX8M MIPI and sub-LVDS Compatibility

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8M MIPI and sub-LVDS Compatibility

Jump to solution
1,998 Views
oneil
Contributor II

Hi,

I am looking to use an i.MX 8M Plus with an image coprocessor. The coprocessor I am using communicates over sub-LVDS MIPI. I am wondering if this signal level is compatible with the MIPI CSI PHY on the i.MX 8M Plus.

It is my understanding that a sub-LVDS driver can drive an LVDS receiver, so since the MIPI CSI interface on the i.MX 8M Plus is just receiving camera data, there should be no issue. Correct?

Thanks

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
1,965 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Yes you are correct!.

Regards

View solution in original post

2 Replies
1,966 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Yes you are correct!.

Regards

1,959 Views
oneil
Contributor II

Thanks for the help!

0 Kudos
Reply