IMX8 PCIE SATA

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8 PCIE SATA

6,045 Views
1074562799
Contributor I

Hi,

         I  have  i.MX 8M Quad Evaluation board. I  want to use  SATA SSD.  So i  conect the ssd to  M.2.

but can't  find the ssd.

         According to the Reference Manual,  it suport pci sata . but how can  i  config to  support sata. is  this have the illustrate  or  have a example  to configure.

         Best regards

0 Kudos
Reply
6 Replies

5,275 Views
jessenchen
Contributor I

HI,Does IMX8M support SSD?If yes, what interfaces are used?

0 Kudos
Reply

5,275 Views
art
NXP Employee
NXP Employee

The i.MX8M processor does not support SATA at all. Only the PCIe interface is available.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

5,275 Views
1074562799
Contributor I

thanks a lot!

0 Kudos
Reply

5,275 Views
传策薛
Contributor V

Hi Artur:

      I  found the configuration of the sata on the imx8m chip data sheet. Is there a bug in the manual?

pastedImage_1.png

0 Kudos
Reply

5,275 Views
art
NXP Employee
NXP Employee

Yes, this is a bug in the manual.

0 Kudos
Reply

5,275 Views
传策薛
Contributor V

I may be mistaken.
What I want to ask is, if you want to support pcie sata, do you need to configure the driver in the kernel?

0 Kudos
Reply