Imx8mq + Androidp9.0 Uboot transplantation?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Imx8mq + Androidp9.0 Uboot transplantation?

1,267 Views
传策薛
Contributor V

Hi community:

     Is there any docs of Imx8mq + Androidp9.0 Uboot custom porting, ddr calibration tool or doc? I already download the "android_p9.0.0_1.0.0-ga_docs.zip",but compared to Android8, Android9's vendor/nxp-opensource/uboot-imx/board/freescale/imx8mq_evk does not have ddr_init.c and ddr_phy.c below?

Labels (1)
0 Kudos
Reply
2 Replies

1,049 Views
igorpadykov
NXP Employee
NXP Employee

Hi 传策 薛 

one can look in documentation included in ddr test

i.MX8 MSCALE SERIES DDR Tool Release (V2.10) 

p.13 MSCALE_DDR_Tool_User_Guide.pdf :
"Press Gen Code button to generate u-boot SPL DDR initialization code. For ‘ARRAY’
format, you can get ‘xxx_timing.c’ in the tool’s directory."
uboot//board/freescale/imx8mq_evk/lpddr4_timing_b0.c

lpddr4_timing_b0.c\imx8mq_evk\freescale\board - uboot-imx - i.MX U-Boot 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,049 Views
传策薛
Contributor V

Thanks:

   Now I get  the "lpddr4_timing.c file", which file should I replace,the "board/freescale/imx8mq_evk/lpddr4_timing.c" or  "lpddr4_timing_b0.c"?

0 Kudos
Reply