IMX8: Audio through qt multimedia module not working

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX8: Audio through qt multimedia module not working

1,783 次查看
vsuneja63
Contributor III

Hi,

Thanks!

Working on imx8mq-evk target. Trying to play audio through qt multimedia but its not working. Could see normal audio files working on target using gst-play also. Added below in local.conf :

PACKAGECONFIG_append_pn-qtmultimedia = " gstreamer"

Is their anything else to be added in the same? 

标签 (1)
0 项奖励
回复
2 回复数

1,734 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello vsuneja63,

Better don't. The current .inc file looks quite different. You might inadvertently replace new code with old one if you do this.

I'd rather try to copy & paste the do_configure_prepend() block into the existing qtmultimedia.inc (unless that block makes no sense anymore). Also, "gstreamer1.0" should be added to the DEPENDS list unless GStreamer 0.10 is built. So, perhaps the gstreamer010 packageconfig line line should be replaced by this:

DEPENDS += "${@bb.utils.contains('PACKAGECONFIG', 'gstreamer010', 'gstreamer gst-plugins-base', 'gstreamer1.0 gstreamer1.0-plugins-base', d)}
Also, note that I use bb.utils.contains instead of base_contains. 

Also there are some threads on the communities regarding issues with EGL in Qt. Have you tried with the Qt5 image from a BSP release? Which image are you baking (over which the local.conf packages are installing)?

Regards

 

0 项奖励
回复

1,759 次查看
vsuneja63
Contributor III

Hi,

Thanks!

Its blocking point for me, any suggestion on this will be highly appreciated.

0 项奖励
回复