IMX7D Ethernet configuration doesn't work on Linux kernel 5.4.200

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX7D Ethernet configuration doesn't work on Linux kernel 5.4.200

5,268 Views
mathad22
Contributor III

Hi there,

I am trying to use the same configuration that works from a Linux kernel 4.14 to a Linux kernel 5.4 but it doesn't :

 

root@hdl-hobc:~# ethtool eth0
Settings for eth0:
Supported ports: [ TP MII ]
Supported link modes: 10baseT/Half 10baseT/Full
100baseT/Half 100baseT/Full
Supported pause frame use: Symmetric
Supports auto-negotiation: Yes
Supported FEC modes: Not reported
Advertised link modes: 10baseT/Half 10baseT/Full
100baseT/Half 100baseT/Full
Advertised pause frame use: Symmetric
Advertised auto-negotiation: Yes
Advertised FEC modes: Not reported
Speed: Unknown!
Duplex: Unknown! (255)
Port: MII
PHYAD: 1
Transceiver: internal
Auto-negotiation: on
Supports Wake-on: g
Wake-on: d
Link detected: no

 

 

From what I see in the logs the libphy doesn't probe the devices.

  • Linux Kernel 4

 

root@hdl-hobc:~# dmesg | grep fec
[    3.369549] fec 30be0000.ethernet: 30be0000.ethernet supply phy not found, using dummy regulator
[    3.407414] fec 30be0000.ethernet (unnamed net_device) (uninitialized): Invalid MAC address: 00:00:00:00:00:00
[    3.417545] fec 30be0000.ethernet (unnamed net_device) (uninitialized): Using random MAC address: 72:4d:f6:20:89:1a
[    3.429237] libphy: fec_enet_mii_bus: probed
[    3.436035] fec 30be0000.ethernet eth0: registered PHC device 0
[    3.443095] fec 30bf0000.ethernet: 30bf0000.ethernet supply phy not found, using dummy regulator
[    3.481159] fec 30bf0000.ethernet (unnamed net_device) (uninitialized): Invalid MAC address: 00:00:00:00:00:00
[    3.491266] fec 30bf0000.ethernet (unnamed net_device) (uninitialized): Using random MAC address: 72:eb:53:5b:c1:d6
[    3.503667] fec 30bf0000.ethernet eth1: registered PHC device 1

 

 

  • Linux Kernel 5:

 

root@hdl-hobc:~# dmesg | grep fec
[    2.927762] fec 30be0000.ethernet: Invalid MAC address: 00:00:00:00:00:00
[    2.934782] fec 30be0000.ethernet: Using random MAC address: e6:c5:f7:eb:6c:81
[    2.955895] fec 30be0000.ethernet eth0: registered PHC device 0
[    2.993873] fec 30bf0000.ethernet: Invalid MAC address: 00:00:00:00:00:00
[    3.000922] fec 30bf0000.ethernet: Using random MAC address: 32:dc:67:04:83:31
[    3.012529] fec 30bf0000.ethernet eth1: registered PHC device 1

 

 

As you can see on kernel 5 the line [ 3.429237] libphy: fec_enet_mii_bus: probed never appears.

 

  • Linux kernel 4 DTS: 

 

&fec1 {
	pinctrl-names = "default";
	pinctrl-0 = <&pinctrl_mdio &pinctrl_enet1>;
	assigned-clocks = <&clks IMX7D_ENET1_REF_ROOT_CLK>,
			  <&clks IMX7D_ENET_AXI_ROOT_SRC>,
			  <&clks IMX7D_ENET1_TIME_ROOT_SRC>,
			  <&clks IMX7D_ENET1_TIME_ROOT_CLK>,
			  <&clks IMX7D_ENET_AXI_ROOT_CLK>;
	assigned-clock-parents = <&clks IMX7D_PLL_ENET_MAIN_50M_CLK>,
				 <&clks IMX7D_PLL_ENET_MAIN_250M_CLK>,
				 <&clks IMX7D_PLL_ENET_MAIN_100M_CLK>;
	assigned-clock-rates = <0>, <0>, <0>, <100000000>, <250000000>;
	clocks = <&clks IMX7D_ENET1_IPG_ROOT_CLK>,
		<&clks IMX7D_ENET_AXI_ROOT_CLK>,
		<&clks IMX7D_ENET1_TIME_ROOT_CLK>,
		<&clks IMX7D_PLL_ENET_MAIN_50M_CLK>,
		<&clks IMX7D_ENET1_REF_ROOT_DIV>;
	phy-mode = "rmii";
	phy-handle = <&ethphy1>;
	mac-address = [ 00 00 00 00 00 00 ];
	local-mac-address = [ 00 00 00 00 00 00 ];
	fsl,magic-packet;
	status = "okay";
	phy-reset-gpios = <&gpio2 0 GPIO_ACTIVE_LOW>;
	phy-reset-duration = <10>;	// 10mS
	phy-reset-post-delay = <10>;	// 10mS

	mdio {
		#address-cells = <1>;
		#size-cells = <0>;
		ethphy1: ethernet-phy@1 {
			compatible = "ethernet-phy-ieee802.3-c22";
			reg = <1>;
			clock-names = "rmii-ref";
			clocks = <&clks IMX7D_PLL_ENET_MAIN_50M_CLK>;
			interrupt-parent = <&gpio1>;
			interrupts = <13 IRQ_TYPE_EDGE_FALLING>;
		};
		ethphy2: ethernet-phy@2 {
			compatible = "ethernet-phy-id0022.1561", "ethernet-phy-ieee802.3-c22";
			reg = <2>;
			clock-names = "rmii-ref";
			clocks = <&clks IMX7D_PLL_ENET_MAIN_50M_CLK>;
			interrupt-parent = <&gpio2>;
			interrupts = <30 IRQ_TYPE_EDGE_FALLING>;
		};
	};
};

&fec2 {
	pinctrl-names = "default";
	pinctrl-0 = <&pinctrl_enet2>;
	assigned-clocks = <&clks IMX7D_ENET2_REF_ROOT_CLK>,
			  <&clks IMX7D_ENET_AXI_ROOT_SRC>,
			  <&clks IMX7D_ENET2_TIME_ROOT_SRC>,
			  <&clks IMX7D_ENET2_TIME_ROOT_CLK>,
			  <&clks IMX7D_ENET_AXI_ROOT_CLK>;
	assigned-clock-parents = <&clks IMX7D_PLL_ENET_MAIN_50M_CLK>,
				 <&clks IMX7D_PLL_ENET_MAIN_250M_CLK>,
				 <&clks IMX7D_PLL_ENET_MAIN_100M_CLK>;
	assigned-clock-rates = <0>, <0>, <0>, <100000000>, <250000000>;
	clocks = <&clks IMX7D_ENET2_IPG_ROOT_CLK>,
		<&clks IMX7D_ENET_AXI_ROOT_CLK>,
		<&clks IMX7D_ENET2_TIME_ROOT_CLK>,
		<&clks IMX7D_PLL_ENET_MAIN_50M_CLK>,
		<&clks IMX7D_ENET2_REF_ROOT_DIV>;
	phy-mode = "rmii";
	phy-handle = <&ethphy2>;
	mac-address = [ 00 00 00 00 00 00 ];
	local-mac-address = [ 00 00 00 00 00 00 ];
	fsl,magic-packet;
	phy-reset-gpios = <&gpio2 1 GPIO_ACTIVE_LOW>;
	phy-reset-duration = <10>;	// 10mS
	phy-reset-post-delay = <10>;	// 10mS
	status = "okay";
};

pinctrl_mdio: mdio-grp {
			fsl,pins = <
				MX7D_PAD_SD2_CD_B__ENET1_MDIO	0x0c
				MX7D_PAD_SD2_WP__ENET1_MDC	0x04
			>;
		};



		pinctrl_enet1: enet1grp {
			fsl,pins = <
				MX7D_PAD_GPIO1_IO13__GPIO1_IO13	0x0c	/* ENET1_nINTid (rev1+) */
				MX7D_PAD_EPDC_DATA00__GPIO2_IO0	0x04	/* ENET1_RST */

				MX7D_PAD_ENET1_RGMII_RX_CTL__ENET1_RGMII_RX_CTL	0x1e
				MX7D_PAD_ENET1_RGMII_RD0__ENET1_RGMII_RD0	0x1e
				MX7D_PAD_ENET1_RGMII_RD1__ENET1_RGMII_RD1	0x1e
				MX7D_PAD_ENET1_RGMII_RXC__ENET1_RX_ER	0x1e
				MX7D_PAD_ENET1_RGMII_TX_CTL__ENET1_RGMII_TX_CTL	0x16
				MX7D_PAD_ENET1_TX_CLK__CCM_ENET_REF_CLK1	0x40000036
				MX7D_PAD_ENET1_RGMII_TD0__ENET1_RGMII_TD0	0x16
				MX7D_PAD_ENET1_RGMII_TD1__ENET1_RGMII_TD1	0x16
			>;
		};

		pinctrl_enet2: enet2grp {
			fsl,pins = <
				MX7D_PAD_EPDC_PWR_COM__GPIO2_IO30	0x0c	/* ENET2_nINTid (rev1+) */
				MX7D_PAD_EPDC_DATA01__GPIO2_IO1	0x04	/* ENET2_RSTidn */

				MX7D_PAD_EPDC_SDCE0__ENET2_RGMII_RX_CTL	0x1e
				MX7D_PAD_EPDC_SDCLK__ENET2_RGMII_RD0	0x1e
				MX7D_PAD_EPDC_SDLE__ENET2_RGMII_RD1	0x1e
				MX7D_PAD_EPDC_SDCE1__ENET2_RX_ER	0x1e
				MX7D_PAD_EPDC_GDRL__ENET2_RGMII_TX_CTL	0x16
				MX7D_PAD_EPDC_BDR0__CCM_ENET_REF_CLK2	0x40000036
				MX7D_PAD_EPDC_SDCE2__ENET2_RGMII_TD0	0x16
				MX7D_PAD_EPDC_SDCE3__ENET2_RGMII_TD1	0x16
			>;
		};

 

 

  • Linux kernel 5, same pinctrl confg:

 

&fec1 {
	pinctrl-names = "default";
	pinctrl-0 = <&pinctrl_mdio &pinctrl_enet1>;

	assigned-clocks = <&clks IMX7D_ENET_PHY_REF_ROOT_SRC>,
			  <&clks IMX7D_ENET_AXI_ROOT_SRC>,
			  <&clks IMX7D_ENET1_TIME_ROOT_SRC>,
			  <&clks IMX7D_ENET1_TIME_ROOT_CLK>,
			  <&clks IMX7D_ENET_AXI_ROOT_CLK>;
	assigned-clock-parents = <&clks IMX7D_PLL_ENET_MAIN_50M_CLK>,
				 <&clks IMX7D_PLL_ENET_MAIN_250M_CLK>,
				 <&clks IMX7D_PLL_ENET_MAIN_100M_CLK>;
	assigned-clock-rates = <0>, <0>, <0>, <100000000>, <250000000>;
	clocks = <&clks IMX7D_ENET1_IPG_ROOT_CLK>,
		 <&clks IMX7D_ENET_AXI_ROOT_CLK>,
		 <&clks IMX7D_ENET1_TIME_ROOT_CLK>,
		 <&clks IMX7D_PLL_ENET_MAIN_50M_CLK>,
		 <&clks IMX7D_ENET1_REF_ROOT_DIV>;

	phy-mode = "rmii";
	phy-supply = <&reg_vref_3v3>;
	phy-reset-gpios = <&gpio2 0 GPIO_ACTIVE_LOW>;
	phy-reset-duration = <10>;	// 10mS
	phy-reset-post-delay = <10>;	// 10mS
	phy-handle = <&ethphy1>;

	mac-address = [ 00 00 00 00 00 00 ];
	local-mac-address = [ 00 00 00 00 00 00 ];
	fsl,magic-packet;
	status = "okay";

	mdio {
		#address-cells = <1>;
		#size-cells = <0>;

		ethphy1: ethernet-phy@1 {
			compatible = "ethernet-phy-ieee802.3-c22";
			reg = <1>;

			clock-names = "rmii-ref";
			clocks = <&clks IMX7D_PLL_ENET_MAIN_50M_CLK>;

			interrupt-parent = <&gpio1>;
			interrupts = <13 IRQ_TYPE_EDGE_FALLING>;
		};

		ethphy2: ethernet-phy@2 {
			compatible = "ethernet-phy-ieee802.3-c22";
			reg = <2>;

			clock-names = "rmii-ref";
			clocks = <&clks IMX7D_PLL_ENET_MAIN_50M_CLK>;

			interrupt-parent = <&gpio2>;
			interrupts = <30 IRQ_TYPE_EDGE_FALLING>;
		};
	};
};

&fec2 {
	pinctrl-names = "default";
	pinctrl-0 = <&pinctrl_enet2>;

	assigned-clocks = <&clks IMX7D_ENET_PHY_REF_ROOT_SRC>,
			  <&clks IMX7D_ENET_AXI_ROOT_SRC>,
			  <&clks IMX7D_ENET2_TIME_ROOT_SRC>,
			  <&clks IMX7D_ENET2_TIME_ROOT_CLK>,
			  <&clks IMX7D_ENET_AXI_ROOT_CLK>;
	assigned-clock-parents = <&clks IMX7D_PLL_ENET_MAIN_50M_CLK>,
				 <&clks IMX7D_PLL_ENET_MAIN_250M_CLK>,
				 <&clks IMX7D_PLL_ENET_MAIN_100M_CLK>;
	assigned-clock-rates = <0>, <0>, <0>, <100000000>, <250000000>;
	clocks = <&clks IMX7D_ENET2_IPG_ROOT_CLK>,
		 <&clks IMX7D_ENET_AXI_ROOT_CLK>,
		 <&clks IMX7D_ENET2_TIME_ROOT_CLK>,
		 <&clks IMX7D_PLL_ENET_MAIN_50M_CLK>,
		 <&clks IMX7D_ENET2_REF_ROOT_DIV>;

	phy-mode = "rmii";
	phy-supply = <&reg_vref_3v3>;
	phy-reset-gpios = <&gpio2 1 GPIO_ACTIVE_LOW>;
	phy-reset-duration = <10>;	// 10mS
	phy-reset-post-delay = <10>;	// 10mS
	phy-handle = <&ethphy2>;

	mac-address = [ 00 00 00 00 00 00 ];
	local-mac-address = [ 00 00 00 00 00 00 ];
	fsl,magic-packet;
	status = "okay";
};

 

 

  • Kernel 4 CLK treeenet-clk-kernel4.png

 

  • Kernel 5 CLK tree​

enet-clk-kernel5.png

Thanks for your help.

Labels (1)
0 Kudos
Reply
5 Replies

4,705 Views
jahM
Contributor I

Did you able to make it work? I am facing the issue of having no link up from kernel 4.19 to 6.23

0 Kudos
Reply

4,701 Views
mathad22
Contributor III

No, I didn't I finally stopped the update to switch from kernel 4 to 6. We will start the update soon, I hope you will find the issue, if you find it I am curious to know the answer. Good luck!

Tags (1)
0 Kudos
Reply

5,133 Views
mathad22
Contributor III
0 Kudos
Reply

5,245 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

You are playing with a non-supported version of the kernel please download a supported version from:

 

https://www.nxp.com/design/design-center/software/embedded-software/i-mx-software/embedded-linux-for...

Regards

 

0 Kudos
Reply

5,162 Views
mathad22
Contributor III

Hi Bio,

Thanks for your answer, I took the Linux FSL to create my branch. Can you please explain me the difference between Linux FSL and Linux IMX ?

I don't get everything. Should I base my branch on Linux IMX ?

For example what version should I use here ? 

https://github.com/Freescale/meta-freescale/blob/dunfell/recipes-kernel/linux/linux-fslc-imx_5.4.bb

https://github.com/Freescale/meta-freescale/blob/dunfell/recipes-kernel/linux/linux-imx_5.4.bb

Thanks,

0 Kudos
Reply