IMX7D - Cortex M4 - GPIO-SPEED

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX7D - Cortex M4 - GPIO-SPEED

1,914 Views
Noel_V
Contributor III

Hi,

At this time I'm trying to determine how fast the CortexM4 can / will handle GPIO reads/writes.

A very simple IO-TOGGLE running on Bare-Metal (native) Cortex-M4.. shows me that it takes up-to +400ns to toggle an GPIO pin.  ( a high low / low high sequence ( square wave) takes +800ns ).

I see similar 'speeds' for reading ( iso writing) an GPIO pin ! 

Is there any possibility to improve ( speed this up) ?

From the reference manual I see that the peripheral clock is running at 24MHz, so I would expect this to be faster ?

Worst case scenario ? Can I increase the peripheral clock speed , without breaking either Linux or FreeRTOS.

Thanks, 

Noel

0 Kudos
Reply
1 Reply

1,724 Views
art
NXP Employee
NXP Employee

The GPIO module switching timings you observe are the realistic ones since these numbers include some software overhead, GPIO inter-module transfer timings etc.

You can try to increase the IPG_CLK_ROOT frequency on your own risk, however, it may cause the whole system to hang up.


Have a great day,
Artur

0 Kudos
Reply