IMX7 ADC question

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,121件の閲覧回数
frankyhsu
Contributor III

Hi

I am checking the ADC input resistance for IMX7 and I found the R_IEXT need to be small to driver the ADC input. Does it mean we need to have 50~250 ohm pull-high to 1.8V and use 10k NTC to GND? Like the below schematic?

pastedImage_3.png

Franky

ラベル(1)
0 件の賞賛
返信
1 解決策
1,735件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi Franky,

Such parameter is not specifically about such hardware configuration (although the idea is maintaining the impedance as low as possible). However, you could refer to the following documents/application notes about ADC parameters and recommendations:

http://www.nxp.com/assets/documents/data/en/application-notes/AN2438.pdf

http://www.nxp.com/assets/documents/data/en/application-notes/AN1058.pdf

http://www.nxp.com/assets/documents/data/en/application-notes/AN4373.pdf

 http://www.nxp.com/assets/documents/data/en/supporting-information/Analog-to-digital-Converter-Train...

Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
1,736件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi Franky,

Such parameter is not specifically about such hardware configuration (although the idea is maintaining the impedance as low as possible). However, you could refer to the following documents/application notes about ADC parameters and recommendations:

http://www.nxp.com/assets/documents/data/en/application-notes/AN2438.pdf

http://www.nxp.com/assets/documents/data/en/application-notes/AN1058.pdf

http://www.nxp.com/assets/documents/data/en/application-notes/AN4373.pdf

 http://www.nxp.com/assets/documents/data/en/supporting-information/Analog-to-digital-Converter-Train...

Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------