IMX7 ADC question

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

IMX7 ADC question

跳至解决方案
2,119 次查看
frankyhsu
Contributor III

Hi

I am checking the ADC input resistance for IMX7 and I found the R_IEXT need to be small to driver the ADC input. Does it mean we need to have 50~250 ohm pull-high to 1.8V and use 10k NTC to GND? Like the below schematic?

pastedImage_3.png

Franky

标签 (1)
0 项奖励
回复
1 解答
1,733 次查看
CarlosCasillas
NXP Employee
NXP Employee

Hi Franky,

Such parameter is not specifically about such hardware configuration (although the idea is maintaining the impedance as low as possible). However, you could refer to the following documents/application notes about ADC parameters and recommendations:

http://www.nxp.com/assets/documents/data/en/application-notes/AN2438.pdf

http://www.nxp.com/assets/documents/data/en/application-notes/AN1058.pdf

http://www.nxp.com/assets/documents/data/en/application-notes/AN4373.pdf

 http://www.nxp.com/assets/documents/data/en/supporting-information/Analog-to-digital-Converter-Train...

Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

1 回复
1,734 次查看
CarlosCasillas
NXP Employee
NXP Employee

Hi Franky,

Such parameter is not specifically about such hardware configuration (although the idea is maintaining the impedance as low as possible). However, you could refer to the following documents/application notes about ADC parameters and recommendations:

http://www.nxp.com/assets/documents/data/en/application-notes/AN2438.pdf

http://www.nxp.com/assets/documents/data/en/application-notes/AN1058.pdf

http://www.nxp.com/assets/documents/data/en/application-notes/AN4373.pdf

 http://www.nxp.com/assets/documents/data/en/supporting-information/Analog-to-digital-Converter-Train...

Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------