IMX7 ADC VREF

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX7 ADC VREF

1,471 Views
thomaskofoedhan
Contributor III

I'm trying to figure out what the VREF for the ADCs is. It is mentioned in table 89 in the datasheet for specifying the input voltage but I can't find the specification for VREF itself.

I'm also looking for some specification from which I can calculate my maximum input impedance. This must have something to do with sample rate etc. as this is ultimately and RC coupling that needs to be charged/discharged. I only intend to measure dc-voltages. 

Labels (2)
0 Kudos
Reply
1 Reply

1,289 Views
Yuri
NXP Employee
NXP Employee

Hello

  The ADC VREF relates to VDDA_ADC1_1P8 and VDDA_ADC2_1P8.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!

0 Kudos
Reply