IMX6q pcie "phy link never came up" on sabresd running mainline 3.14.0-rc2

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX6q pcie "phy link never came up" on sabresd running mainline 3.14.0-rc2

3,224 次查看
bdauvin
Contributor I

Hi, I was going through this thread and I am having a similar issue:

pcie "phy link never came up" on sabresd running dora 3.10.17_beta

I am running on a sabresd board and I have enabled the pcie in the device tree but the phy link is not coming up properly.  I've gone through a few threads online but I am having trouble finding an answer for the mainline kernel.  Any ideas as to what I can try to resolve this situation? USB SUPPORT is enabled in my .config file but I am still having this issue.

Thanks,

Ben

Here are some logs and messages:

# dmesg | grep "pci"

imx6q-pcie 1ffc000.pcie: phy link never came up

pci_bus 0000:00: root bus resource [io  0x1000-0x10000]

pci_bus 0000:00: root bus resource [mem 0x01000000-0x01efffff]

pci_bus 0000:00: No busn resource found for root bus, will use [bus 00-ff]

pci 0000:00:00.0: [16c3:abcd] type 01 class 0x060400

pci 0000:00:00.0: reg 0x10: [mem 0x00000000-0x000fffff]

pci 0000:00:00.0: reg 0x38: [mem 0x00000000-0x0000ffff pref]

pci 0000:00:00.0: supports D1

pci 0000:00:00.0: PME# supported from D0 D1 D3hot D3cold

pci_bus 0000:01: busn_res: [bus 01-ff] end is updated to 01

pci_bus 0000:00: busn_res: [bus 00-ff] end is updated to 01

pci 0000:00:00.0: BAR 0: assigned [mem 0x01000000-0x010fffff]

pci 0000:00:00.0: BAR 6: assigned [mem 0x01100000-0x0110ffff pref]

pci 0000:00:00.0: PCI bridge to [bus 01]

pci 0000:00:00.0: PCI bridge to [bus 01]

pci_bus 0000:00: resource 4 [io  0x1000-0x10000]

pci_bus 0000:00: resource 5 [mem 0x01000000-0x01efffff]

pcieport 0000:00:00.0: Signaling PME through PCIe PME interrupt

pcie_pme 0000:00:00.0:pcie01: service driver pcie_pme loaded

# lspci

00:00.0 Class 0604: 16c3:abcd

标签 (2)
标记 (1)
4 回复数

1,804 次查看
YixingKong
Senior Contributor IV

Ben

This discussion is closed since no activity. If you still need help, please feel free to reply with an update to this discussion, or create another discussion.

Thanks,

Yixing

0 项奖励
回复

1,804 次查看
YixingKong
Senior Contributor IV

Ben

Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help, please feel free to reply with an update to this discussion.

Thanks,

Yixing

0 项奖励
回复

1,804 次查看
fabio_estevam
NXP Employee
NXP Employee

Ben,

Could you try 3.15-rc3 instead? There have been many new patches improving mx6 pci lately.

If you still see issues, please report  it to linux-arm-kernel mailing list.

0 项奖励
回复

1,804 次查看
gusarambula
NXP TechSupport
NXP TechSupport

The thread you mentioned (https://community.freescale.com/thread/320124) is still ongoing so I would suggest following it.

Once an answer has been posted please let them know in that same thread if it does/doesn’t work so it gets follow up.

0 项奖励
回复