IMX6ULL Linux 5.15 - EPIT

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6ULL Linux 5.15 - EPIT

Jump to solution
4,040 Views
Jeroen_H
Contributor III

Hi,

I'm using an iMX6ULL and trying to use the EPIT timer as a timersource for my application.

All I can find in the NXP Linux manuals is this:

Jeroen_H_1-1711700627567.png

But, this file doesn't exist in the kernel source tree, so I'm not sure how to use this.

 

So, basically I'm looking for some hints, examples or starting points to use the EPIT timer in Linux 5.15.

Thanks!

Jeroen.

 

 

Labels (2)
Tags (1)
0 Kudos
Reply
1 Solution
4,025 Views
joanxie
NXP TechSupport
NXP TechSupport

pls check the mail I sent to you for reference

View solution in original post

0 Kudos
Reply
3 Replies
4,026 Views
joanxie
NXP TechSupport
NXP TechSupport

pls check the mail I sent to you for reference

0 Kudos
Reply
3,956 Views
Jeroen_H
Contributor III

Hi Joanxie,

Thank you!
I've updated the patch for 5.15.x, and can confirm the timer is running and generates interrupts.

It’s still a bit unclear how proceed from that point on to use the timer from a userspace application, like setting the timeout interval and receiving an interrupt with e.g. a select()-call.

Do you perhaps also have a small example of that?

Thanks again,

Jeroen.

0 Kudos
Reply
3,925 Views
Jeroen_H
Contributor III

Already succeeded using EPIT in userland.

Example not necessary anymore.

0 Kudos
Reply