IMX6UL ethernet does work in u-boot but it doesn't with Kernel 3.14.38

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

IMX6UL ethernet does work in u-boot but it doesn't with Kernel 3.14.38

跳至解决方案
13,094 次查看
alubeiro
Contributor IV

Hi everybody,

My partner Goiatz Leibar and me are facing this issue.

First of all, say we have a customized board with the IMX6UL processor. and with the kernel 3.14.38-6UL

The fact is that we got ethernet working in u-boot but not in kernel.

We use ENET1 and as we also use the GPIO1_IO06 and GPIO1_IO07 for other purposses, the MDIO and MDC are in "ENET2_RX_DATA0 and ENET2_RX_DATA1"

 

In U-BOOT (working fine)

This are the chages so ethernet works in u-boot.

We select FEC 0, (mx6ul_14x14_evk.h)

144144_144144.pngpastedImage_2.png

We change the MDIO and MDC pins (mx6ul_14x14_evk.c)

144143_144143.pngpastedImage_0.png

In Kernel

But when we try to make it works in kernel, we do the following with no succsses

In kernel's device tree (imx6ul14x14-evk.dts):

We disable FEC2 and we also add our board pins

 

144145_144145.pngpastedImage_8.png

 

144152_144152.pngpastedImage_13.png

 

 

Once the system has booted, we make an "ifconfig -a" and here you can see how MAC address is the one we asigned before in u-boot.

 

144153_144153.pngpastedImage_14.png

 

Please find attached the .log file when the board boots

Original Attachment has been moved to: Custom_boot.txt.zip

标签 (2)
1 解答
6,812 次查看
LuisCasado
NXP Employee
NXP Employee

Hello Alberto Lubeiro ,

If you disable FEC2, you need to add mdio to FEC1, like this:

&fec1 {

               pinctrl-names = "default";

               pinctrl-0 = <&pinctrl_enet1>;

               phy-mode = "rmii";

               phy-handle = <&ethphy0>;

               status = "okay";

               mdio {

                              #address-cells = <1>;

                              #size-cells = <0>;

                              ethphy0: ethernet-phy@2 {

                                             compatible = "ethernet-phy-ieee802.3-c22";

                                             reg = <2>;

                              };

                              ethphy1: ethernet-phy@1 {

                                             compatible = "ethernet-phy-ieee802.3-c22";

                                             reg = <1>;

                              };

               };

};

&fec2 {

               pinctrl-names = "default";

               pinctrl-0 = <&pinctrl_enet2>;

               phy-mode = "rmii";

               phy-handle = <&ethphy1>;

               status = "disabled";

};

And this change in the FEC1 pins:

                              pinctrl_enet1: enet1grp {

                                             fsl,pins = <

                                                            MX6UL_PAD_ENET1_RX_EN__ENET1_RX_EN       0x1b0b0

                                                            MX6UL_PAD_ENET1_RX_ER__ENET1_RX_ER        0x1b0b0

                                                            MX6UL_PAD_ENET1_RX_DATA0__ENET1_RDATA00               0x1b0b0

                                                            MX6UL_PAD_ENET1_RX_DATA1__ENET1_RDATA01               0x1b0b0

                                                            MX6UL_PAD_ENET1_TX_EN__ENET1_TX_EN        0x1b0b0

                                                            MX6UL_PAD_ENET1_TX_DATA0__ENET1_TDATA00               0x1b0b0

                                                            MX6UL_PAD_ENET1_TX_DATA1__ENET1_TDATA01               0x1b0b0

                                                            MX6UL_PAD_ENET1_TX_CLK__ENET1_REF_CLK1 0x4001b031

                                                            MX6UL_PAD_GPIO1_IO06__ENET1_MDIO           0x1b0b0

                                                            MX6UL_PAD_GPIO1_IO07__ENET1_MDC                            0x1b0b0

                                             >;

                              };

These changes disable FEC2 in EVK and FEC1 works.

Luis

在原帖中查看解决方案

7 回复数
6,813 次查看
LuisCasado
NXP Employee
NXP Employee

Hello Alberto Lubeiro ,

If you disable FEC2, you need to add mdio to FEC1, like this:

&fec1 {

               pinctrl-names = "default";

               pinctrl-0 = <&pinctrl_enet1>;

               phy-mode = "rmii";

               phy-handle = <&ethphy0>;

               status = "okay";

               mdio {

                              #address-cells = <1>;

                              #size-cells = <0>;

                              ethphy0: ethernet-phy@2 {

                                             compatible = "ethernet-phy-ieee802.3-c22";

                                             reg = <2>;

                              };

                              ethphy1: ethernet-phy@1 {

                                             compatible = "ethernet-phy-ieee802.3-c22";

                                             reg = <1>;

                              };

               };

};

&fec2 {

               pinctrl-names = "default";

               pinctrl-0 = <&pinctrl_enet2>;

               phy-mode = "rmii";

               phy-handle = <&ethphy1>;

               status = "disabled";

};

And this change in the FEC1 pins:

                              pinctrl_enet1: enet1grp {

                                             fsl,pins = <

                                                            MX6UL_PAD_ENET1_RX_EN__ENET1_RX_EN       0x1b0b0

                                                            MX6UL_PAD_ENET1_RX_ER__ENET1_RX_ER        0x1b0b0

                                                            MX6UL_PAD_ENET1_RX_DATA0__ENET1_RDATA00               0x1b0b0

                                                            MX6UL_PAD_ENET1_RX_DATA1__ENET1_RDATA01               0x1b0b0

                                                            MX6UL_PAD_ENET1_TX_EN__ENET1_TX_EN        0x1b0b0

                                                            MX6UL_PAD_ENET1_TX_DATA0__ENET1_TDATA00               0x1b0b0

                                                            MX6UL_PAD_ENET1_TX_DATA1__ENET1_TDATA01               0x1b0b0

                                                            MX6UL_PAD_ENET1_TX_CLK__ENET1_REF_CLK1 0x4001b031

                                                            MX6UL_PAD_GPIO1_IO06__ENET1_MDIO           0x1b0b0

                                                            MX6UL_PAD_GPIO1_IO07__ENET1_MDC                            0x1b0b0

                                             >;

                              };

These changes disable FEC2 in EVK and FEC1 works.

Luis

6,813 次查看
harveydueck
Contributor I

I have a similar board, but the hardware guys made two more changes:

- PHY address changed to 1

- ENET1_nRST (the phy reset line) moved to GPIO2 IO10

My device tree changes are shown below, but ethernet is still not working in linux.  Ethernet works from u-boot after changing CONFIG_FEC_ENET_DEV to 0.

The ethernet link light goes out at roughly the same time the "configuring network interfaces" message appears on the console:

Configuring network interfaces... fec 20b4000.ethernet eth0: Freescale FEC PHY driver [Micrel KSZ8081 or KSZ8091] (mii_bus:phy_addr=20b4000.ethernet:01, irq=-1)

IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready

Any suggestions about how to fix this?

Here are the relevant parts of my device tree (added phy-reset-gpios, changed phy address to 1 and added MDC and MDIO to pinctrl_enet1):

&fec1 {

        pinctrl-names = "default";

        pinctrl-0 = <&pinctrl_enet1>;

        phy-mode = "rmii";

        phy-handle = <&ethphy0>;

        phy-reset-gpios = <&gpio2 10 0>; /* GPIO2_10, pin B14  */

        status = "okay";

        mdio {

                #address-cells = <1>;

                #size-cells = <0>;

                ethphy0: ethernet-phy@1 {

                        compatible = "ethernet-phy-ieee802.3-c22";

                        reg = <1>;

                };

        };

};

...

                pinctrl_enet1: enet1grp {

                        fsl,pins = <

                                MX6UL_PAD_ENET2_RX_EN__GPIO2_IO10       0x0b0b0     /* ENET1_nRST (phy reset) */

                                MX6UL_PAD_GPIO1_IO07__ENET1_MDC         0x1b0b0

                                MX6UL_PAD_GPIO1_IO06__ENET1_MDIO        0x1b0b0

                                MX6UL_PAD_ENET1_RX_EN__ENET1_RX_EN      0x1b0b0

                                MX6UL_PAD_ENET1_RX_ER__ENET1_RX_ER      0x1b0b0

                                MX6UL_PAD_ENET1_RX_DATA0__ENET1_RDATA00 0x1b0b0

                                MX6UL_PAD_ENET1_RX_DATA1__ENET1_RDATA01 0x1b0b0

                                MX6UL_PAD_ENET1_TX_EN__ENET1_TX_EN      0x1b0b0

                                MX6UL_PAD_ENET1_TX_DATA0__ENET1_TDATA00 0x1b0b0

                                MX6UL_PAD_ENET1_TX_DATA1__ENET1_TDATA01 0x1b0b0

                                MX6UL_PAD_ENET1_TX_CLK__ENET1_REF_CLK1  0x4001b031

                        >;

                };

0 项奖励
回复
6,813 次查看
compmas2
Contributor V

Harvey,

Correct me if I am wrong but isn't the reset line on the PHY active low? If so then use the following line to setup the reset:

phy-reset-gpios = <&gpio2 10 GPIO_ACTIVE_LOW>; /* GPIO2_10, pin B14  */

You had <&gpio2 10 0> which is active high. It is recommended to use the GPIO_ACTIVE_HIGH and GPIO_ACTIVE_LOW defines instead of 0 and 1 to avoid confusion.

0 项奖励
回复
6,813 次查看
harveydueck
Contributor I

Matthew, thanks for the quick reply.

The phy reset is indeed active low.  However, ethernet still doesn't work after making the change.  I checked the RST pin with a scope and it's high, so the PHY is not being held in reset.

0 项奖励
回复
6,813 次查看
jiriluznicky
Contributor III

Look closely at your PHY chip and check the P/N. Even the minor change on third line means change in id. And there is a bug in imx6ul fix to support this phy driver. In file arch/arm/mach-imx/mach-imx6ul.c in function __init imx6ul_enet_phy_init(void) bad mask is used in PHY id check phy_register_fixup_for_uid(PHY_ID_KSZ8081, 0xffffffff, ksz8081_phy_fixup); . You can try to fix it by chaging the mask to 0xffffff00 or include linux/micrel_phy.h and use MICREL_PHY_ID_MASK to fix it correctly.

6,813 次查看
harveydueck
Contributor I

Thank you, Jiri!  That fixes my problem.

I included linux/micrel_phy.h and used MICREL_PHY_ID_MASK in arch/arm/mach-imx/mach-imx6ul.c and ethernet now comes up in linux. 

0 项奖励
回复
6,813 次查看
alubeiro
Contributor IV

Hi Luis,

Thanks! we have just added it and it works!

Thanks again and best regards.

0 项奖励
回复