Hello All,
I need my ADC driver working in the imx6ul board with 9 channels.
I have modified dtsi files as shown below:
adc1: adc@02198000 {
 compatible = "fsl,imx6ul-adc", "fsl,vf610-adc";
 reg = <0x02198000 0x4000>;
 interrupts = <GIC_SPI 100 IRQ_TYPE_LEVEL_HIGH>;
 clocks = <&clks IMX6UL_CLK_ADC1>;
 num-channels = <9>;
clock-names = "adc";
 status = "disabled";
 };
pinctrl_adc1: adc1grp {
fsl,pin = <
 MX6UL_PAD_GPIO1_IO00__GPIO1_IO00 0xb0
 MX6UL_PAD_GPIO1_IO01__GPIO1_IO01 0xb0
 .
.. .
 .
 MX6UL_PAD_GPIO1_IO07__GPIO1_IO07 0xb0
 MX6UL_PAD_GPIO1_IO08__GPIO1_IO08 0xb0
 >;
};
 
 &adc1 {
 pinctrl-names = "default";
 pinctrl-0 = <&pinctrl_adc1>;
 vref-supply = <®_mba6ul_3v3>;
 status = "okay";
};
but i am getting the voltage as 4095 all the times when i am varying the input volatges
and in boot logs i am getting below print for adc.
imx6ul-pinctrl 20e0000.iomuxc: no fsl,pins property in node /soc/aips-bus@02000000/iomuxc@020e0000/imx6ul-mba6ul/adc1grp
So, I tried adding one of the pin(GPIO1_IO01) configuration under "lcdifgrp" and the voltage was varying for the particular channel.
Similary, we added all the pins under "lcdifgrp".
All channel voltages except one(GPIO4_IO04) was varying.
Could someone tell me what might be the issue?
Kindly help to resolve this .
Regards,
Anshul
Hi Anshul
one can check if GPIO4_IO04 used in uboot and look at issue described on
iMX6UL adc calibration fails 
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Igor,
Thank you for the reply,
I have checked GPIO1_IO04 is not using in uboot,
but i am not able to vary the voltage value on the pin.
what could be be the issue??
kindly help to resolve this .
Regards,
Anshul
Hi Anshul
to check if this is not hardware issue, please try to reproduce it
on i.MX6UL EVK reference board.
Best regards
igor