IMX6UL-ADC issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6UL-ADC issue

2,709件の閲覧回数
anshulkhare
Contributor III

Hello All,

I need my ADC driver working in the imx6ul board with 9 channels.

I have modified dtsi files as shown below:

adc1: adc@02198000 {
compatible = "fsl,imx6ul-adc", "fsl,vf610-adc";
reg = <0x02198000 0x4000>;
interrupts = <GIC_SPI 100 IRQ_TYPE_LEVEL_HIGH>;
clocks = <&clks IMX6UL_CLK_ADC1>;
num-channels = <9>;

clock-names = "adc";
status = "disabled";
};

pinctrl_adc1: adc1grp {

fsl,pin = <
MX6UL_PAD_GPIO1_IO00__GPIO1_IO00 0xb0
MX6UL_PAD_GPIO1_IO01__GPIO1_IO01 0xb0
.
.. .
.
MX6UL_PAD_GPIO1_IO07__GPIO1_IO07 0xb0
MX6UL_PAD_GPIO1_IO08__GPIO1_IO08 0xb0
>;

};

&adc1 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_adc1>;
vref-supply = <&reg_mba6ul_3v3>;
status = "okay";
};

but i am getting the voltage as 4095 all the times when i am varying the input volatges
and in boot logs i am getting below print for adc.

imx6ul-pinctrl 20e0000.iomuxc: no fsl,pins property in node /soc/aips-bus@02000000/iomuxc@020e0000/imx6ul-mba6ul/adc1grp


So, I tried adding one of the pin(GPIO1_IO01) configuration under "lcdifgrp" and the voltage was varying for the particular channel.
Similary, we added all the pins under "lcdifgrp".
All channel voltages except one(GPIO4_IO04) was varying.
Could someone tell me what might be the issue?

Kindly help to resolve this .

Regards,

Anshul

ラベル(1)
タグ(3)
0 件の賞賛
返信
3 返答(返信)

2,205件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Anshul

one can check if GPIO4_IO04 used in uboot and look at issue described on
iMX6UL adc calibration fails 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,205件の閲覧回数
anshulkhare
Contributor III

Hello Igor,

Thank you for the reply,
I have checked GPIO1_IO04 is not using in uboot,
but i am not able to vary the voltage value on the pin.


what could be be the issue??
kindly help to resolve this .

Regards,
Anshul

0 件の賞賛
返信

2,205件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Anshul

to check if this is not hardware issue, please try to reproduce it

on i.MX6UL EVK reference board.

Best regards
igor

0 件の賞賛
返信