IMX6UL ADC differential Inputs

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX6UL ADC differential Inputs

952 次查看
shammi112
Contributor I

Hello,

Does imx6ul internal ADC has differential inputs ?

Thanks & Regards,

SHAMMI

0 项奖励
回复
1 回复

851 次查看
CarlosCasillas
NXP Employee
NXP Employee

Hi SHAMMI,

In case of the i.MX6UL processor, it has up to two 12-bit ADC modules with up to 10 input channels in total. However, all the channels are single ended; it doesn’t include differential inputs.

You could find a test procedure in the ADC Driver chapter of i.MX Linux Manual document.


Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复