IMX6UL ADC differential Inputs

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6UL ADC differential Inputs

987件の閲覧回数
shammi112
Contributor I

Hello,

Does imx6ul internal ADC has differential inputs ?

Thanks & Regards,

SHAMMI

0 件の賞賛
返信
1 返信

886件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi SHAMMI,

In case of the i.MX6UL processor, it has up to two 12-bit ADC modules with up to 10 input channels in total. However, all the channels are single ended; it doesn’t include differential inputs.

You could find a test procedure in the ADC Driver chapter of i.MX Linux Manual document.


Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信