IMX6SX JTAG TOOL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,648件の閲覧回数
2548903578
Contributor III

Hi!

   I am using the IMX6SX chip recently and have bought a development board from the official website. I see JTAG on the development board. I just want to ask which JTAG tools this chip supports.

IMG_20200828_104058.jpg

Is this tool OK?

ラベル(1)
0 件の賞賛
返信
1 解決策
1,634件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi ZXS

I think it can support

Multilink | Debug Probe | PEmicro 

however may be useful to confirm it posting question on vendor forum:

Multilink | Debug Probe | PEmicro 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,635件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi ZXS

I think it can support

Multilink | Debug Probe | PEmicro 

however may be useful to confirm it posting question on vendor forum:

Multilink | Debug Probe | PEmicro 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信