IMX6S Display Error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6S Display Error

1,930 Views
giorgiosoldavin
Contributor I

Good morning,

I'm using Android 4.0.4 on BCM board based on IMX6S. I'm actually facing with problem on LVDS display: after at least one day running, randomly display go black (usually with orange vertical lines) but applications (checking by ADB) are still working..

The error I can catch throurgh Android Log is:

<fb_post, 184> ioctl FBIOPAN_DISPLAY failed


Can anyone please help me?

Thank you for the support.

BR

Giorgio

Labels (4)
0 Kudos
Reply
2 Replies

1,800 Views
igorpadykov
NXP Employee
NXP Employee

Hi Giorgio

FBIOPAN_DISPLAY error is Android frame buffer error,

caused by bug on some Android ports. You may contact bcmcom.com for

more updated Android release. Alternatively you can post this to meta-fsl-arm

mailing list, so that someone familiar with this board could try to assist you.

https://lists.yoctoproject.org/listinfo/meta-freescale

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,800 Views
giorgiosoldavin
Contributor I

Hi Chip,

yes, thank you; BCM already provide me a newer Android version.

I'm asking because, at the moment, I don't want to use the latest version because on actual AOSP version I've made a lot of customization that would take a lot of time to be ported on new one.

Because of this, I'm investigating if there are some patches to be applied to Android 4.0.4 that could solve the problem.

Anyway, again thank you for your reply.

BR

Giorgio

0 Kudos
Reply