IMX6Q- vpu encoder CBR setting

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX6Q- vpu encoder CBR setting

2,319 次查看
krishnachandrap
Contributor I

Hi,

I just wanted to know the chip capability of imx6q VPU for CBR mode. I have been setting the CBR of 2.5M bits/sec but the vlc shows the bit rate of 4M bits/sec whenever there is a motion. 

imxvpuenc_h264‌ imx vpu‌ imxstreaming‌ imx6qvpuCBR‌ imx6quad

标签 (2)
2 回复数

2,181 次查看
joanxie
NXP TechSupport
NXP TechSupport

refer to the vpu refence manual, The bitrate should be between 0 and 32767.

2,181 次查看
krishnachandrap
Contributor I

Hi Joan Xie,

Our problem is : Even though we have set CBR as 2560 kbps our output stream is showing higher bit rate of 4500 - 5000 kbps as read using vlc player. Our understanding was that our output bit rate would not exceed the CBR set (10% tolerance is acceptable) but this was not observed practically as mentioned above.

Could you please tell us how to restrict encoded output bit rate below the CBR set (+/- 10% tolerance)? 

Following are the some of the parameters that we have configured

  1.         gopSize : 20 
  2.        . sliceMode : 1
  3.        . sliceSizeMode : 1
  4.        . sliceSize : 360
  5.          MESearchRange : 1 
  6.          bitRate : 2560
0 项奖励
回复