IMX6Q overheat issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6Q overheat issue

2,206件の閲覧回数
zhaobing
Contributor I

Hi,all

       we are developing product with IMX6Q processor MCIMX6Q6AVT10AC & PMIC MMPF0100F0EP.

the attachment is block diagram of my application

When Video input through CSI0 of IMX6Q processor, at the same time  Video is playing through LCD_DI0 of IMX6Q processor ;CPU and PMIC  is heating to much. VDDSOC_IN drop to 1.2V, the video is not play. the input current is always hold 2.37A of 4.2V of PMIC.Meanwhile ,the console may input command. if you reboot or reset the cpu , the roofs  crash.

But when I power down system  power and CPU 's the quantity of heat  drop away, the system  boot up is normal.

But When Video input through CSI0 of IMX6Q processor, at the same time  Video is playing through HDMI of IMX6Q processor , the CPU and PMIC temperature is normal. the video is play normal.

IMX6Q overheat issue appear is random,the probability is 5%.

We measured all of voltage of CPU, only PMIC Voltage output to  SOC is reducing to 1.20V, as a result VDDSOC_CAP and VDDPU_CAP is drop to 1.0V.The others are normal.

What might be the issue , How can it be handled in Software and Hardware ?

ラベル(5)
0 件の賞賛
返信
1 返信

1,967件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi zhao

if issue happens only with LCD, you can test

with removed LCD and check.

Reason may be in high processor high loading with LCD,

due to long cable or (probably) termination resistors.

Best regards

igor

0 件の賞賛
返信