IMX6Q Yocto project fail

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6Q Yocto project fail

ソリューションへジャンプ
4,172件の閲覧回数
dt_liumi
Contributor I

Dear:

I configure the yocto project as shown in Figure 1 ,

repo init -u https://source.codeaurora.org/external/imx/fsl-arm-yocto-bsp.git -b imx-morty -m imx-4.9.11-1.0.0_ga.xml

repo sync

DISTRO=fsl-imx-x11 MACHINE=imx6qsabresd source fsl-setup-release.sh -b build-x11

bitbake fsl-image-qt5-validation-imx

The error is shown in Figure 2

Best regards

thank you 

0 件の賞賛
返信
1 解決策
4,158件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello dt_liumi,

You can download another BSP, because the L4.9.11 is out of support since it tries to download the firmware from freescale,com and that´s the fails. you can download the BSP from:

https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applicat...

 

Regards

 

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
4,159件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello dt_liumi,

You can download another BSP, because the L4.9.11 is out of support since it tries to download the firmware from freescale,com and that´s the fails. you can download the BSP from:

https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applicat...

 

Regards

 

 

0 件の賞賛
返信