IMX6Q USB OTG IN DEVICE MODE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6Q USB OTG IN DEVICE MODE

1,976件の閲覧回数
mauriziomontesi
Contributor I

Hello. I'm designing a new custom board based on IMX6Q processor. My board will use USB OTG only for serial boot so in "device mode". I never will use host mode of OTG. Following my question:

1) I use mini USB B receptacle connector, and I left the  USB_OTG_ID always pulled up inside the board. 

2) On USB mini B connector I leave +5V pin unconnected, and I connect th USB_OTG_VBUS on IMX6 to the +5VCC internal voltage (generated internally the board).

3) The only connections on mini B USB connector are USB_OTG_DN, USB_OTG_DP and USB_OTG_GND .

Is that correct for a OTG in a fixed "Device " mode?

Regards

Maurizio

ラベル(1)
2 返答(返信)

1,268件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Maurizio

I think this is correct connections.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,268件の閲覧回数
mauriziomontesi
Contributor I

Thanks a lot Igor

Regards

Maurizio

0 件の賞賛
返信