how to know imx6 vpu current frequency and how to increase it ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how to know imx6 vpu current frequency and how to increase it ?

2,970件の閲覧回数
nagendrasarma
Contributor III

hi All

i am using imx6dual and 3.10.17 kernel

i would like to know about VPU

how to know the current frequency of VPU ? and how to increase and what is maximum supported?

0 件の賞賛
返信
5 返答(返信)

2,020件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

Maximum supported trhoughput,  is 72,576,000 pixels /s @ VPU frequency of 266 mhz

2 x  1024 x 600 x 60hz = 73,728,000

And you can refer to  VPU max frequency in our community.
Have a great day,
Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Mark Correct  button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,020件の閲覧回数
mcergun
Contributor III

why did you multiply the result with 2 in the beginning?

2 x 1024 x 600 x 60

0 件の賞賛
返信

2,020件の閲覧回数
nagendrasarma
Contributor III

Hi,  NXP

I am using IMX6 dual module  with the vpu firmware file "vpu_fw_imx6q.bin (md5 af2a9be3c6cf797afd8e8bf7a8c4a654)"

and able to encode 

but I am experiencing a strange behavior while streaming the encoded h264 data through RTPH264PAY plugin and decoding with VLC (2.2.4)   

at every 35 to 45 mins, the decoder (vlc-media-player) displays warning  "can not decode one frame" , do you have any idea about this ?

i tried to use firmware vpu_fw_imx6d.bin (d4a0fc04c9d7f5f5b114fb8c60566f53)  which is not working throwing version mismatch error.

is vpu firmware is correct ? if yes, why there are two firmware with files ? even though my module is dual, it is working with vpu_fw_imx6q.bin but not with vpu_fw_imx6d.bin, what is the difference between them ?

0 件の賞賛
返信

2,020件の閲覧回数
nagendrasarma
Contributor III

hi  Dan

thanks for reply.

i am using imx6 dual, for HD and SD video encoding and streaming,

i found some frame losses with dual stream,  i would like to increase vpu freq to 325Mhz and test.

i did not get clear picture how to increase clock to 325MHZ

i am using 3.10.17 kernel

please let me know how to increase vpu to 325mhz

regards

nagendra

0 件の賞賛
返信

2,020件の閲覧回数
nagendrasarma
Contributor III

Hi   All

i am using following patch (3.10.17) to increase my VPU frequency to 352Mhz

and my vddsoc and vddpu showing

vddpu: 725 <--> 1450 mV at 1150 mV

vddsoc: 725 <--> 1450 mV at 1200 mV

please let me know how to increase these voltages to 1250 mv (required for VPU) ?

patch used to increase vpu freq.

753 #ifdef CONFIG_MX6_VPU_352M

754         /*

755          * If VPU 352M is enabled, then PLL2_PDF2 need to be

756          * set to 352M, cpufreq will be disabled as VDDSOC/PU

757          * need to be at highest voltage, scaling cpu freq is

758          * not saving any power, and busfreq will be also disabled

759          * as the PLL2_PFD2 is not at default freq, in a word,

760          * all modules that sourceing clk from PLL2_PFD2 will

761          * be impacted.

762          */

763         imx_clk_set_rate(clk[pll2_pfd2_396m], 352000000);

764         imx_clk_set_parent(clk[vpu_axi_sel], clk[pll2_pfd2_396m]);

765         pr_info("VPU 352M is enabled!\n");

766 #endif

regards

nagendra

0 件の賞賛
返信