IMX6Q MfgTool burn program failed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6Q MfgTool burn program failed

2,503 Views
tommyduan
Contributor III

We use Mfgtool burn program ,it stop"jumping to os image",can't going on!How can we find the reason?before it's ok,Where should I look for the reason?How does the burning process run?How does the system process work after startup?

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

2,294 Views
igorpadykov
NXP Employee
NXP Employee

Hi tommy

stop"jumping to os image" may mean that board can not run mfg tool

since ddr settings are wrong for that board. It s necessary to run ddr test

i.MX6/7 DDR Stress Test Tool V2.92 

https://community.nxp.com/docs/DOC-328258 

and rebuild mfg tool with new ddr settings found from ddr test.

For example one can look on

How to build MFG Firmware for i.MX6Q 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply