IMX6Q IPU scale

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX6Q IPU scale

4,890 次查看
richarddestiny
Contributor III

Hi,ALL

      I‘m working on IMX6Q kernel version:3.10.17

     my sensor output is 1280*1080+25FPS

    I want to know, can I scale the resolution to 1280*960 or 1280*720,not crop.if it work,how to do?

thank for your reply~~

0 项奖励
回复
8 回复数

4,447 次查看
saurabh206
Senior Contributor III

Hi Richard,

Which BSP are you using?

If you are using LINUX BSP than you can find gstreamer based pipeline for Camera content encoding.

Thanks

Saurabh

0 项奖励
回复

4,447 次查看
richarddestiny
Contributor III

Hi,dear Saurabh

   I‘m using Linux bsp version:yocto 3.10.17,but I can't get the document about gstreamer-plugins for 3.10.17, whether gstreamer-plugins for 3.0.35 is ok?

can your give me  some help to make me work faster .thanks

0 项奖励
回复

4,447 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  Hope the following helps ipu-examples release notes - v0.1

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

4,447 次查看
richarddestiny
Contributor III

Hi,dear Yuri

     I need to scale the video stream and then encode it by vpu, Is it will be work?

any example?

0 项奖励
回复

4,447 次查看
Yuri
NXP Employee
NXP Employee

> I need to scale the video stream and then encode it by vpu, Is it will be work?

Yes, Gstreamer using is good approach to do it.

Regards,

Yuri.

0 项奖励
回复

4,447 次查看
richarddestiny
Contributor III

Hi,dear Saurabh

   I‘m using Linux bsp version:yocto 3.10.17,but I can't get the document about gstreamer-plugins for 3.10.17, whether gstreamer-plugins for 3.0.35 is ok?

can your give me  some help to make me work faster .thanks

0 项奖励
回复

4,447 次查看
saurabh206
Senior Contributor III

Hi Richard,

You can do IPU scaling according to your requirement.

You can refer mxc_v4l2_tvin test.

You can add support for the IPU task.

Thanks

Saurabh

0 项奖励
回复

4,447 次查看
richarddestiny
Contributor III

Hi,dear Saurabh

     I need to scale the video stream and then encode it by vpu, Is it will be work?

any example?

0 项奖励
回复