SABRE for Automotive Infotainment - i.MX 6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SABRE for Automotive Infotainment - i.MX 6

388 Views
erikgrant
Contributor I

Hi,

  We're working with an i.MX 6 series SABRE board and had a question regarding the included JTAG adapter.  We're trying to locate a schematic for the adapter so we can see what the pin assignments are.  We've got the schematics for the CPU card but have not had any luck in locating one for the adapter.  Is one available?  Thanks.

Labels (5)
0 Kudos
1 Reply

340 Views
Yuri
NXP Employee
NXP Employee

Hello,

  The i.MX6 provides standard JTAG interface, that may be used either

for Boundary Scan (IEEE1149.1) or for software JTAG debugging.
Please refer to i.MX6 Reference Manual(s) for more details about

the JTAG interface. NXP / FSL designs use standard (20-pin) connector

for it, which is intended for external Emulators/Probes.

Please look at corresponding section of the i.MX6  Design tool Web : 

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos