IMX6Q IDE and compiler tools

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6Q IDE and compiler tools

ソリューションへジャンプ
2,898件の閲覧回数
naveenb
Contributor II

Hi, 

We have started our design using IMX6 quad processor, we are in Hardware design stage and wanted to start software application design parallely now.

I wanted to know the IDE to be used which supports the Application, Image processing (OpenCV) and Graphical user interface (OpenGl).

It would be great if anyone reply back ASAP.

Thanks!

0 件の賞賛
返信
1 解決策
2,617件の閲覧回数
naveenb
Contributor II
0 件の賞賛
返信
2 返答(返信)
2,617件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

 You may look at the following Summary Page regarding recommended software

i.MX 6 Series Software and Development Tool|NXP

  NXP Linux BSP supports QT5 (please use Linux BSP documentation for more details),

therefore it makes sense to use QT5 features and tools.

Installing and Configuring QT Creator (Ubuntu) 

Computer Vision on i.MX Processors: Building OpenCV-2.4.X for Freescale's i.MX6 BSP (Yocto) 

Qt | Cross-platform software development for embedded & desktop 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,618件の閲覧回数
naveenb
Contributor II

Thanks!

0 件の賞賛
返信